Skip to main content
dsystem
Associate II
April 12, 2018
Question

BLDC Motor Control in Torque Mode

  • April 12, 2018
  • 1 reply
  • 686 views
Posted on April 12, 2018 at 12:24

I am working on project using STEVAL-SPIN3201 board with SDK4.3.0.

I am able to control in speed mode. 

I want to know procedure to Read Present torque, How to set Torque value and How to Relate it with Current.

Secondly when I use commands related to Torque, like:

Run_Torque = MCI_GetTorque(oMCI[0]); 

I get error

error:  &sharp167: argument of type 'CMCI' is incompatible with parameter of type 'CSTC'

Also I want to Change mode during run time. How to do it ??

Regards

Vimal Amin

#bldc-torque-mode
This topic has been closed for replies.

1 reply

Laurent Ca...
Senior III
June 15, 2021

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards