Skip to main content
brianbrian9
Associate
July 30, 2013
Question

ST7FLITE29 Write Protect

  • July 30, 2013
  • 1 reply
  • 699 views
Posted on July 30, 2013 at 12:08

Hi

I have a new build PCB with a ST7Flite29 fitted, I cant program the device, I have had to run an external clock signal to Clk In (PB4), the programmer is now reporting ''Write Protected'', how do I get this back, the ERASE device is greyed out on the STVP programmer

Regards, Brian
This topic has been closed for replies.

1 reply

LaurentL
ST Employee
August 12, 2013
Posted on August 12, 2013 at 14:39

Hello,

Normally, a brand new ST7 should not be write protected.

Anyway, in STVP, read option bytes and then just change the option bit FMP_W ''WRITE protection'' to OFF and reprogram the options bytes.

Then, you can reprogram the program memory.(If the FMP_R is OFF too).

Rgds,

Laurent

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.