Skip to main content
josef2
Associate III
February 2, 2018
Question

STM32L4x2 Multimaster mode of UART

  • February 2, 2018
  • 0 replies
  • 445 views
Posted on February 02, 2018 at 11:03

Hi,

is it possible to set the STM32L4x2 UART to a 9 bit address mode, where only the 9th bit create an interrupt or wake up from mute mode. Actually I see the only possibility to set only one address. But in some protocols there are not only one address but for example as a second a sync byte on the bus or a general call (0x7e or 0x7f), where all slaves has to hear.

best regards and thank's a lot.

J. Baumann

    This topic has been closed for replies.