I'm using Sourcery G++ Lite 2010q1-188 here. I had problems with a later free version.
Also keep in mind the support for debugger/flasher. I don't think ST-Link works in Linux, so you'll either have to upload firmware through UART (ISP) or with a openocd compatible JTAG dongle (there are a bunch in 50eur range). Other than that, I'm happily developing on stm32 under Linux since 2008 :)
It's probably an uphill battle as there isn't the same commercial drive.
As for a GCC/GNU compiler, the STM32 code can be built with CodeSourcery arm-2007q3-53-arm-none-eabi Lanchon, and Martin Thomas have done work in this area, so examples, makefiles and linker scripts can be found on the net.
Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
''The only tricky part of using stlink-download is that it does only what you tell it to do.''
I would say that's exactly how it should be!
Far too many things try to be ''helpful'' (sic) by trying to anticipate what they think you want - but this just ends up getting in the way and making them inflexible!''For instance, you must explicitly erase the Flash before downloading a new program.''
A perfect example: it might think that it would be ''helpful'' (sic) to automatically erase the Flash before downloading - but that would then prevent you from doing anything that required, say, part of the flash to be left intact...!
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
I typically use Ubuntu, and it was only a matter of downloading a few packages to get a working GCC compile environment.
Working with the STLink was a different level of effort altogether. I ended up looking at the protocol and writing my own 'stlink-download' program, which I've put up on Google Code. The only tricky part of using stlink-download is that it does only what you tell it to do. For instance, you must explicitly erase the Flash before downloading a new program.