Skip to main content
waclawek.jan
Super User
January 2, 2018
Question

['F446 documentation] SAI clock generator

  • January 2, 2018
  • 1 reply
  • 1036 views
Posted on January 02, 2018 at 23:49

The SAI clock generator subchapter and related comments throughout the SAI chapter are confusing. A complete rewrite would be beneficial, but I doubt anybody is willing to do that. So let me give a couple of simple suggestions:

- the figure ought to contain the SCK-to-FS divider; and the MCLK-to-SCK divider should indicate that its division rate is 256/FRL+1; such figure then would present a complete clock information (for free protocol setting + master).

In fact, you already have that figure; I don't see why RM contains an inferior and confusing version:

0690X00000609KJQAY.png

- similarly, the formula for SCK frequency shall read MCLK/(256/(FRL+1)), as the multiplication form confusingly suggests that there is some ''multiplier'' present; and accompanying text should point out that this strange arrangement is designed so that FS is always MCLK/256. The confusing ''In the SAI, the single ratio MCLK/FS = 256 is considered.'' sentence could then be removed

- the text ''In master mode it is mandatory that (FRL[7:0] +1) is equal to a number with a power of 2'' should be accompained by pointing out the safeguard mechanism in form of WCKCFG

- MCLK stops to be output when MCKDIV=0 and FRL=255; the RM shall say this either in this subchapter, or at FRL bits description; or maybe both, as it's quite surprising.

- in Configuration register 1 (SAI_ACR1 / SAI_BCR1) , description of MCKDIV contains an incorrect formula (the result is not F

SCK_x

)

JW

    This topic has been closed for replies.

    1 reply

    waclawek.jan
    Super User
    January 16, 2018
    Posted on January 16, 2018 at 12:55

    To the last item: that formula is incorrect for FREE, but may be correct for SPDIF; however, it should explicitly say so.

    https://community.st.com/0D50X00009XkaCESAZ

    JW