Skip to main content
Mikk Leini
Senior
Mar 9, 2015 8:32 AM UTC
Question

PMSM FOC SDK 4.0 code stucks

Posted on March 09, 2015 at 09:32

Hello,

I can't get PMSM library working. I don't have motor evaluation board, i have self-built board with STM32F303RB and i have F3 discovery. Problem is that program gets lost in library instructions and ends up stuck on strange memory addresses. I have tried Keil u-Vision and IAR EWARM examples with same results. I have tried it on three computers.

Does anybody have a clue why it should stuck?

I have asked it here also: 

/public/STe2ecommunities/mcu/Lists/STM32Java/Flat.aspx?RootFolder=https://my.st.com/public/STe2ecommunities/mcu/Lists/STM32Java/PMSM%20FOC%20code%20stuck&FolderCTID=0x01200200770978C69A1141439FE559EB459D758000F9A0E3A95BA69146A17C2E80209ADC21&currentviews=35

I have some specific questions also:

Does it matter what Keil or IAR version to use? Should i use the same versions as the library is built with?

Has anybody got the PMSM FOC SDK 4.0 working with their own F3 MCU's?

#stm32f3-psms-foc-stuck
This topic has been closed for replies.

3 replies

Gigi
ST Employee
Mar 9, 2015 9:27 AM UTC
Posted on March 09, 2015 at 10:27

Ciao

Please verify that the LCD functionality is not enabled in the ST MC Workbench project.

And also verify that the emercency input of the micro (TIMx_BRK2) is not active (usually pulled up) at the begining of execution of MC.

Ciao

Gigi

Mikk Leini
Senior
Mar 13, 2015 8:30 PM UTC
Posted on March 13, 2015 at 21:30

I found multiple reasons why my custom project stucked. They are written in first post.

Laurent Ca...
Senior III
Jun 17, 2021 8:18 AM UTC

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards