Question
Single motor on ADC3/4
Posted on March 11, 2015 at 22:52
Hello,
Does the PMSM FOC library support single motor drive using OPAMP3/4 and ADC3/4 on STM32F303RB?I did my own HW like that but it seems that the library still tries to check some flags of ADC1 even if none of the signals are connected to ADC1 nor 2.PMSM manual says: the pair OPAMP3/OPAMP4 can be used additionally in a project based on STM32F303.What does this ''additionally'' mean? That it's the second option or that it supports second motor? #pmsm-single-drive-adc34 #opamp3\4 #foc4.1 #stm32f303