Skip to main content
flyer31
Senior
November 2, 2012
Question

STM32F4xx.H error: DBGMCU_APB2... not correctly defined

  • November 2, 2012
  • 2 replies
  • 1566 views
Posted on November 02, 2012 at 08:09

In STM32F4xx.H the bits DBGMCU_APB2... are erroneously named DBGMCU_APB1... - just info.

    This topic has been closed for replies.

    2 replies

    Tesla DeLorean
    Guru
    November 2, 2012
    Posted on November 02, 2012 at 11:02

    These ones

    /******************** Bit definition for DBGMCU_APB2_FZ register ************/
    #define DBGMCU_APB1_FZ_DBG_TIM1_STOP ((uint32_t)0x00000001)
    #define DBGMCU_APB1_FZ_DBG_TIM8_STOP ((uint32_t)0x00000002)
    #define DBGMCU_APB1_FZ_DBG_TIM9_STOP ((uint32_t)0x00010000)
    #define DBGMCU_APB1_FZ_DBG_TIM10_STOP ((uint32_t)0x00020000)
    #define DBGMCU_APB1_FZ_DBG_TIM11_STOP ((uint32_t)0x00040000)

    Thanks for the FYI
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Nickname12657_O
    Associate III
    January 3, 2013
    Posted on January 03, 2013 at 11:42

    Hi Bil,

    It is noted, thanks for information!

    Cheers,

    STONe-32