Skip to main content
flyer31
Senior
November 24, 2012
Question

long long in interrupts: how to write safe in main? (disable int or semaphore?)

  • November 24, 2012
  • 1 reply
  • 581 views
Posted on November 24, 2012 at 15:09

Hi,

please have a look at the following code (STM32F407):

volatile long long vllPosition;

void TIM1_UP_TIM10_IRQHandler(void){

... do interrupt stuff ...

vllPosition ++;

... do interrupt stuff ...

}

int main( void){

  ... do some init stuff ...

  for(;;){

    ... do the loop stuff ...

    if( ...){        // from time to time it is necessary to assing some value to llPosition

      vllPosition= llSomeValue;

    }

    ... do the loop stuff ...

  }

}

As long long is 64 bit, the access to vllPosition is non-atomic. So an assignment like vllPosition= llSomeValue is dangerous: it might be interrupted by my interrupt and then the complete thing will mix up.

In an easy access, I would like to disable the interrupt temporarily. There would be 3 different possibilities I see:

1.:

      NVIC_DisableIRQ( TIM1_UP_TIM10_IRQn);

      vllPosition= llSomeValue;

      NVIC_EnableIRQ( TIM1_UP_TIM10_IRQn);

2. (The TIM1_UP_TIM10_IRQ is entered exclusively by the UIE):

      TIM1->DIER = 0;

      vllPosition= llSomeValue;

      TIM1->DIER = TIM_DIER_UIE;

 

3.

      __disable_irq();

      vllPosition= llSomeValue;

      __enable_irq();

 

Is any of these methods 100% safe (of course I would prefer method 1 or 2, as 3 disables all interrupts)? (Due to the prefetch delay I am not sure about this - I did not find a guarantee anywhere and it is difficult to decide only by testing). (Or would I need some more elaborate methode to ensure this in a secure way, e. g. with semaphores or so?)

#stm32
    This topic has been closed for replies.

    1 reply

    flyer31
    flyer31Author
    Senior
    November 24, 2012
    Posted on November 24, 2012 at 17:00

    I found it meanwhile in the ARM docs:

    The Disable in (1.) needs an additional ISB and DSB instruction, see

    http://infocenter.arm.com/help/index.jsp?topic=/com.arm.doc.dai0321a/BIHHFHJD.html

    (''4.6 Disabling Interrupts using NVIC'')

    The Disable in (2.) is NOT recommended, see

    http://infocenter.arm.com/help/index.jsp?topic=/com.arm.doc.dai0321a/BIHHFHJD.html

    (''4.9 Disabling interrupts at peripherals'')

    The Disable in (3.) works without ISB and DSB - but of course it stops all interrupts:

    siehe:

    http://infocenter.arm.com/help/index.jsp?topic=/com.arm.doc.dai0321a/BIHHFHJD.html

    (''4.8. Disabling interrupts using CPS and MSR instructions'')