Skip to main content
dhoyen
Associate II
September 16, 2008
Question

str912 : Timer connected with 2 source interrupt at the same time

  • September 16, 2008
  • 2 replies
  • 656 views
Posted on September 16, 2008 at 07:27

str912 : Timer connected with 2 source interrupt at the same time

This topic has been closed for replies.

2 replies

dhoyen
dhoyenAuthor
Associate II
May 17, 2011
Posted on May 17, 2011 at 09:55

Well,

After few test,

He seems it's working....

No problem from this side, excepting the library...

Regards.

damien

dhoyen
dhoyenAuthor
Associate II
May 17, 2011
Posted on May 17, 2011 at 09:55

Hi everybody,

Question about timer:

When a clear timer is done (TIM_CounterCmd(TIM0, TIM_CLEAR)), the register will be set to a reset value : 0xFFFC. (maybe somebody from ST can explain me this choice of design :D )

Means: if before, I have enabled an interrupt for the TO,

i will receive a interrupt during the roll from 0xFFFF to 0, immediately after the call of the function: timer clear followed by a start, is it correct ?

By the same, I would know if everybody already tried to connect 2 Timer source of interrupt (ex : ICAP1 and TO) at the same time to a unique Timer?

Is it working ?

In my case seems something wrong in the timer library (look code after: ST lib v2.0) : Impossible to set more than 1 interrupt at the same time.

Is it a silicium limitation, or just a error during the writing of the library ?

Thanks in advance.

Any comments welcome.

Damien.

void TIM_ITConfig(TIM_TypeDef *TIMx, u16 TIM_IT, FunctionalState TIM_Newstate)

{

if(TIM_Newstate == ENABLE)

{

/* TIMx->CR2 = (TIMx->CR2 & 0x00FF) | TIM_IT; */

 

// previous code will remove a previously installed interrupt,

 

// Why this choice ?

 

TIMx->CR2 |= TIM_IT;

 

[ This message was edited by: dhoyen on 12-09-2008 12:15 ]

[ This message was edited by: dhoyen on 12-09-2008 14:36 ]