Skip to main content
dhoyen
Associate II
September 16, 2008
Question

Problem ARM912: DMA and ADC sems not working

  • September 16, 2008
  • 4 replies
  • 890 views
Posted on September 16, 2008 at 08:57

Problem ARM912: DMA and ADC sems not working

This topic has been closed for replies.

4 replies

dhoyen
dhoyenAuthor
Associate II
May 17, 2011
Posted on May 17, 2011 at 09:55

Hi all,

I try to connect my ADC with a DMA access to push in memory, the result of a unique channel, but for an important number of sample .

 

Problem:

 

 

When i read the register DDR, in my ADC interrupt

 

the registre DDR (ADC->DDR) is always 0.

This register should receive something else...

Especially because my channel 5 receive something like 1.5-2v.

I can read 0x212 with the ADC->DR5 register, which is absolutely normal

I have activated the ADC_DMA mode : via ADC_DMACmd(ENABLE);

 

Is somebody have already experienced this problem ?

 

Could be a silicium limitation?

If somebody have already realized this operation, what is the value for the field :

DMA_InitStruct.DMA_Channel_FlowCntrl

 

DMA_InitStruct.DMA_Channel_Des

 

DMA_InitStruct.DMA_Channel_Src

 

(i don't know really between DMA_FlowCntrl_Perip2 or DMA_FlowCntrl2_DMA, and i have some trouble with the documentation)

thanks in advance.

Damien.

For the test, I m running my ADC in continuous mode,

Clock Peripheral, before prescaler : 48 Mhz (Look Init code)

My demo board is with a STR912FW44X6, silicon B (little bit old, but mounted by default). Compil: GCC / Yagarto

---- Init

ADC_Setup.ADC_Channel_5_Mode = ADC_NoThreshold_Conversion;

ADC_Setup.ADC_Select_Channel = ADC_Channel_5;

ADC_Setup.ADC_Scan_Mode = DISABLE;

ADC_Setup.ADC_Conversion_Mode = ADC_Continuous_Mode;

ADC_PrescalerConfig(128);

/* Enable DMA for ADC*/

ADC_DMACmd(ENABLE);

---- Interrupt -----

static u16 DMAData;

static u16 ConvertResult;

if (ADC_GetFlagStatus (ADC_FLAG_ECV) == SET )

{

ADC_ClearFlag (ADC_FLAG_ECV);

DMAData = ADC->DDR; // <- Receive always 0

ConvertResult = ADC->DR5; // <- Receive 0x212

}

dhoyen
dhoyenAuthor
Associate II
May 17, 2011
Posted on May 17, 2011 at 09:55

Well,

he seems the silicon version, present in my demo board

 

: STR912F W44X6 (not A)... is limited.

 

The ADC Timer trigger is only available for rev A.

 

Same code running on a STR911FA W44X6 (A) seems work (TBC)

regards

dhoyen
dhoyenAuthor
Associate II
May 17, 2011
Posted on May 17, 2011 at 09:55

Hi rgreenthal,

Thanks for your help.

I tried to change the ADC->DDR register to the adress of the ADC->DR5 Register. Problem is I don't know really how the ADC will be able to generate a DMA request transfert if this DDR register don't works.

I tried to generate myself in the interrupt ADC end of convertion

a DMA request, via these function :

DMA_SetSReq (DMA_External_Req1_Mask);

DMA_SetBReq (DMA_External_Req1_Mask);

But nothing, no data is written in my destination buffer, stay with init value.

Any idea welcome.

Damien

rgreenthal
Associate III
May 17, 2011
Posted on May 17, 2011 at 09:55

Need to setup Linked Lists for the received data buffer, like this for SSP

(change SSP0_BASE+2 to your input, i.e. ADC->DR5 (ADC_BASE+offset))

// Receive Control Link List

StructLinkList LLRxBuffer = {

(long*)SSP0_BASE+2, // source pointer

(long*)&usNetRxBuffer[0], // destination

(long*)&LLRxBuffer, // rotating buffer

// Channel Control

(long) DMA_DesIncrement // destination increment, NewFWLib name

| DMA_SrcWidth_HalfWord // source 16 bits

| DMA_DesWidth_HalfWord // destination 16 bits

| RX_BUFFER_SIZE, // length

// Channel Configuration

(long) DMA_FlowCntrl2_DMA // flow control

| DMA_SRC_SSP0_RX // source SSP0 receive

};

Also need to load this by using

ExecLinkList(DMA_Channel0, &LLRxBuffer);

where

/***********************************

Configure Channel and Execute

ExecLinkList(DMA_Channel0, &LLFpRxBuffer);

ExecLinkList(DMA_Channel1, &LLFpTxCommand);

ExecLinkList(DMA_Channel2, &LLNetRxBuffer);

ExecLinkListLength(DMA_Channel3, &LLNetTxCommand, nLength);

************************************/

void ExecLinkList(DMA_Channel_TypeDef * Channel, StructLinkList * LinkList)

{

// Channel->CCNF &= ~DMA_ChannelEnable;

DMA_ChannelCmd(Channel, DISABLE);

Channel->SRC = (long)LinkList->p_lSource;

Channel->DES = (long)LinkList->p_lDest;

Channel->LLI = (long)LinkList->p_lNextList;

Channel->CC = (long)LinkList->lControl;

// CCNF not part of link list

Channel->CCNF = (long)LinkList->lConfig;

// Channel->CCNF |= DMA_ChannelEnable;

DMA_ChannelCmd(Channel, ENABLE);

} // End of Function ''ExecLinkList()''