Skip to main content
joe239955_stm1
Associate
January 18, 2012
Question

L6470 Application Note???

  • January 18, 2012
  • 2 replies
  • 719 views
Posted on January 18, 2012 at 16:49

The L6470 works well but seem to have a lot of quirks.

Do you have any idea when the real application note will be available?

 Joe

From therad ''EVAL6470 operation via SPI''

Posted: 5/17/2011 10:20 AM

Enrico Poli

''Finally, I want to highlight that the AN3103 is not the L6470 one, it is the description of the dSPIN evaluation environment only. The official AN of the product is under development.''

Posted: 5/17/2011 10:20 AM

Enrico Poli

''- We are not allowed to distribute draft versions of application notes.''
This topic has been closed for replies.

2 replies

Enrico Poli
ST Employee
February 3, 2012
Posted on February 03, 2012 at 10:44

Dear Joe,

Sorry for the waiting.

The AN about the new voltage mode driving will be shortly released, but we not have an official date.

I will create a post in the forum as soon as it is released.

Anyway the forum and the online support is at your disposal for any support request and clarifications.

Thanks for your patience.

Enrico

greg239955_st
Visitor II
September 3, 2012
Posted on September 03, 2012 at 02:49

Enrico,

Any updates?  I'm part of a project where we're considering using this part, but the unusual interface requirements and lack of solid documentation are leading us to explore other solutions.  It's too bad, because initially, this looks like a great solution.

Thanks for any info!

Greg