Skip to main content
mwp
Associate III
March 22, 2018
Question

[bug] SysTick_Handler optimised out of F4 HAL project

  • March 22, 2018
  • 3 replies
  • 837 views
Posted on March 22, 2018 at 19:52

Hi all,

So i've been banging my head up against a wall trying to work out what's been going on here...

Somehow SysTick_Handler() and so HAL_IncTick() are being optimized out (or just not included) in my Release build.

The code/project runs just fine on the target STM32F401 when complied as a Debug build.

When built as a Release build (gcc options are below), the jump location for int15 (SysTick) is the Default_Handler.

I cant understand why this is happening. The HAL libraries are unmodified, and the 

HAL_IncTick() increments uwTick which is a volatile uint_32. I do use HAL_Delay(), so uwTick is referred to in the normal running of the program.

Has anyone come across this problem before?

The Release GCC options are:

arm-none-eabi-gcc -mcpu=cortex-m4 -mthumb -mfloat-abi=soft -Os -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections -fno-common -ffreestanding -fsingle-precision-constant -flto -Wall -Wno-discarded-qualifiers  -DSTM32F4 -DSTM32F401xC -DUSE_HAL_DRIVER -DUSE_FULL_LL_DRIVER -DHSE_VALUE=16000000  -std=gnu11 -Wbad-function-cast

GCC version is:

arm-none-eabi-gcc (GNU Tools for Arm Embedded Processors 7-2017-q4-major) 7.2.1 20170904 (release) [ARM/embedded-7-branch revision 255204]

Cube is latest version as of today, Cube F4 package version is: stm32cube_fw_f4_v1210.zip

#systick #stm32
This topic has been closed for replies.

3 replies

mwp
mwpAuthor
Associate III
March 22, 2018
Posted on March 22, 2018 at 20:20

To add to this...

Ive temporarily fixed the issue by commenting out the following lines in system_xxx.s:

.weak SysTick_Handler

.thumb_set SysTick_Handler,Default_Handler

I'm now having the same problem with the USB OTG int handler, so its not just limited to SysTick.

Any ideas?

Tesla DeLorean
Guru
March 22, 2018
Posted on March 22, 2018 at 20:37

Sounds more of an issue with the linker or linker script than being Cube's fault.

I'd start by looking if/why the vector table isn't being included or placed. An then the symbol attributes for the offending functions in objects they do exist in.

If C++ files or settings are being used watch out for name mangling, or explicitly use extern 'C' on the IRQ Handlers

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
mwp
mwpAuthor
Associate III
March 23, 2018
Posted on March 23, 2018 at 18:33

Yes, you're right, it does appear to be a gcc/ld problem.

There is no C++ in this project at all, so that should not be the issue.

Using the previous version of the arm-gcc toolset fixes the problem.