Skip to main content
Franzi.Edo
Senior
November 20, 2017
Solved

L1 cache for stm32H743

  • November 20, 2017
  • 4 replies
  • 1379 views
Posted on November 20, 2017 at 20:53

Dear all,

I am trying to set-up a new board using an stm32H743.

In my tests, I initialized the MPU in order to use the cache L1 with the Flash.

When I initialize the MPU to use the cache, the results are really impressive (about 1.8 faster than without L1).

Unfortunately, the system is not stable; I often have 'hardfault' situation.

Any suggestion of how to use L1 with the internal Flash?

Here is my initialization code before activating the cache.

Best regards

  Edo

 ...

// New attributes for the FLASH area (0x08000000)

// Change the attribute only in the executable area

   MPU->CTRL = 0x00000000;    // Disable the MPU

   MPU->RNR  = 0x00000000;    // Region 0

   MPU->RBAR = 0x08000000 | (1<<4) | (0<<0); // Address, valid & region 0

   MPU->RASR = (0<<28)    // Instruction fetches enabled

            | (6<<24)     // Unprivileged read-only

            | (0<<19)     // TEX: 000 Memory attribute

            | (1<<18)     // S: 0

            | (1<<17)     // C: 1

            | (0<<16)     // B: 0 un-sharable, Normal, outer and inner write-through,

                          //      no write allocate

            | (0<<8)      // Corresponding sub-region is enabled

            | (20<<1)     // 2-MB

            | (1<<0);     // Region enable

  MPU->CTRL = (1<<2)      // Enable the usage of all the default map

             | (1<<1)     // MPU is enabled during the fault

             | (1<<0);    // MPU enabled

   MEMO_SYNC_BARRIER;

   DATA_SYNC_BARRIER;

   INST_SYNC_BARRIER;

   ...

#stm32h7
This topic has been closed for replies.
Best answer by Franzi.Edo
Posted on November 20, 2017 at 23:42

Solved! It seems necessary to initialize the MPU segment for the RAM area used by the system (in my case the RAM of 512-KBytes). I don't know yet why, but it works. Without this initialization the RAM is not reliable and the system crashes.

Best regards

  Edo

4 replies

Franzi.Edo
Franzi.EdoAuthorBest answer
Senior
November 20, 2017
Posted on November 20, 2017 at 23:42

Solved! It seems necessary to initialize the MPU segment for the RAM area used by the system (in my case the RAM of 512-KBytes). I don't know yet why, but it works. Without this initialization the RAM is not reliable and the system crashes.

Best regards

  Edo

Evgeny Erlihman
Associate III
November 21, 2017
Posted on November 21, 2017 at 22:39

Hi Edo,

Why did you have to enable MPU in-order to enable L1 cache? Cant't L1 data/instruction cache be enabled while the MPU is disabled?

Thanks,

Evgeny

waclawek.jan
Super User
November 21, 2017
Posted on November 21, 2017 at 23:09

In Cortex-M7, it's the MPU which governs the cache. Read AN4839 .

JW