Associate III
June 5, 2018
Solved
Over the Air Update BLE, STM32F2, CRC Always 0?
- June 5, 2018
- 5 replies
- 1566 views
Posted on June 05, 2018 at 17:21
I would suggest opening the file attached in notepad++.
Generally speaking the code makes sense. I can get it working without the CRC, which apparently is supposed to equal 0.
Note the following section:
if(psFirmware->ulPage == (psFirmware->ulTotalPages - 1)){
sFirmware.ucRcvdImage = TRUE; //verify FW if(sFirmware.ucUpdateWhat == fwUPDATE_CONSOLE){ ulCRC_Calc = sFirmware.ulFirstWord; sFirmware.ulAddress = UPDATE_IMAGE_ADDRESS+4; size = ((psFirmware->ulTotalPages * 12) /4)-1; }else{ ulCRC_Calc = 0; sFirmware.ulAddress = UPDATE_RADIO_ADDRESS; size = ((psFirmware->ulTotalPages * 12) /4); } for(i = 0x000 ; i < size ; i++){ ulMemoryRead = *(__IO uint32_t*)sFirmware.ulAddress; sFirmware.ulAddress += 4; ulCRC_Calc += ulMemoryRead; //ADD the bits to calculate the checksum } if(1){//ulCRC_Calc == 0){ //verify FW image here if(sFirmware.ucUpdateWhat == fwUPDATE_CONSOLE){ FlashStatus = FLASH_ProgramWord(UPDATE_IMAGE_ADDRESS,sFirmware.ulFirstWord); if(FlashStatus != FLASH_COMPLETE){ while(1); } firmwareUpdateProc(keyFW_RESET); }else{ sFirmware.ulTotalBytes = (psFirmware->ulTotalPages * 12); firmwareUpdateRadio(); } }else{ firmwareEraseUpdateSectors(); NVIC_SystemReset(); } }The code above is saying (if I get rid of the if(1)) that the CRC of the first word, plus all of the words written to flash for the image of the app, should be 0.
I have no clue why this is the case. Is it just standard for the MCU to place a value in the application address that should work this way?
Thank you for your support,
Daniel