Question
5V & 3V3 POWER SUPPLY BAT60 DIODES: are they critical ?
Posted on May 20, 2013 at 12:11
Hello,
I'm currently designing my own schematic based on the STM32F4DISCOVERY board.The two BAT60 power supply protection diodes (D1 & D3) are not relevant for me because they generate a dropout voltage: +5V is in fact +4.7V and +3.3V is +3V.I want a full +5V to supply my analog functions (based on opamps) and a full +3.3V to allow the STM32F407 to generate/convert 3.3V signals with the DAC/ADC. (my only board power supply is the USB VBUS)Are the BAT60 really critical concerning the USB power supply protection ? I need to remove them...Thanks !