Skip to main content
totally
Associate II
December 9, 2012
Question

STM32F4 Discovery Accelerometer SPI Problem

  • December 9, 2012
  • 17 replies
  • 3226 views
Posted on December 09, 2012 at 14:41

Hello,

I'm trying to get the MEMS Accelerometer on my STM32F4 Discovery Board to run with a simple code, but I don't make it.

Heres my code:

int main(void)

{

        SystemInit();

        GPIO_InitTypeDef GPIO_InitStructure;

        SPI_InitTypeDef  SPI_InitStructure;

        RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOD | RCC_AHB1Periph_GPIOA | RCC_AHB1Periph_GPIOE , ENABLE);

        RCC_APB2PeriphClockCmd(RCC_APB2Periph_SPI1, ENABLE);

          //Init SPI-Pins

          GPIO_InitStructure.GPIO_Pin = GPIO_Pin_5 | GPIO_Pin_6 | GPIO_Pin_7;

          GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;

          GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;

          GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;

          GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;

          GPIO_Init(GPIOA, &GPIO_InitStructure);

          //Init CS-Pin

          GPIO_InitStructure.GPIO_Pin = GPIO_Pin_3;

          GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT;

          GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;

          GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;

          GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;

          GPIO_Init(GPIOE, &GPIO_InitStructure);

          GPIO_SetBits(GPIOE, GPIO_Pin_3);  //Set CS high

          GPIO_PinAFConfig (GPIOA, GPIO_PinSource5 |GPIO_PinSource6 |GPIO_PinSource7 , GPIO_AF_SPI1);

          SPI_I2S_DeInit(SPI1);

          SPI_InitStructure.SPI_Direction = SPI_Direction_2Lines_FullDuplex;

          SPI_InitStructure.SPI_Mode = SPI_Mode_Master ;

          SPI_InitStructure.SPI_DataSize = SPI_DataSize_16b ;

          SPI_InitStructure.SPI_CPOL = SPI_CPOL_High    ;

          SPI_InitStructure.SPI_CPHA = SPI_CPHA_2Edge;

          SPI_InitStructure.SPI_NSS = SPI_NSS_Soft ;

          SPI_InitStructure.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_32;

          SPI_InitStructure.SPI_FirstBit = SPI_FirstBit_MSB;

          SPI_InitStructure.SPI_CRCPolynomial = 0;

          SPI_Init(SPI1, &SPI_InitStructure);

          SPI_Cmd(SPI1, ENABLE);

          GPIO_ResetBits(GPIOE, GPIO_Pin_3);

          SPI_I2S_SendData(SPI1, 0x20C7);    //Sensor Config

    while(1){

        //Read Y-Axis

        SPI_I2S_SendData(SPI1, 0xAB00);

        SPI_I2S_ReceiveData(SPI1);

    }

I'm running this in Debug-mode only (step by step), so there should not be any timing problems due to missing flag-status requests.

After sending the data, RXNE bit in SPI SR Register is set but the SPI Data Register always contains 0x0000. I have also tried different modes changing CPOL and CPHA, no results.

I am using CooCox IDE

I hope somebody can help!

Thanks,

Alex.

#accelerometer #stm32f4 #spi #metoo
This topic has been closed for replies.

17 replies

Tesla DeLorean
Guru
December 9, 2012
Posted on December 09, 2012 at 17:18

GPIO_PinAFConfig (GPIOA, GPIO_PinSource5 |GPIO_PinSource6 |GPIO_PinSource7 , GPIO_AF_SPI1);

Not going to work, PinSource is an index, not a bit vector. Break into multiple lines.
Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
totally
totallyAuthor
Associate II
December 9, 2012
Posted on December 09, 2012 at 17:38

Cool, thanks a lot! Works fine now

amirpatel7625
Visitor II
July 17, 2013
Posted on July 17, 2013 at 15:11

Hi

does this code work? I've been struggling for 2 days to read the accelerometer data and I keep just getting 0xFF in my out rexeived buffer.

 

Am I doing something wrong?

Tesla DeLorean
Guru
July 17, 2013
Posted on July 17, 2013 at 16:40

Am I doing something wrong?

Apparently.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
ahsankhushe
Associate
August 28, 2013
Posted on August 28, 2013 at 19:50

Hi

Can any one tell me how to get the acceleration value ? I want to calculate the distance by using it.

Thanks.

crt2
Visitor II
August 29, 2013
Posted on August 29, 2013 at 10:03

Above code with small correction gets you a number out. Distance through acceleration? This is something we can discuss about nicely. You do know that acceleration is 0 when speed is constant? This might get you into problem - just a thought.

ahsankhushe
Associate
August 29, 2013
Posted on August 29, 2013 at 10:22

Yes, i know this fact but what about if we store the previous acceleration and when speed becomes constant we can use that previously stored value of acceleration ?

crt2
Visitor II
August 29, 2013
Posted on August 29, 2013 at 12:58

Honestly by asking this question my only response can be: go check the basic physics book again. What you could do is calculate speed or something and go with that...

frankmeyer9
Associate III
August 29, 2013
Posted on August 29, 2013 at 14:37

Reducing the requirements from ''odometer'' to ''step counter'' would make it sound more realistic ...

randyao12345
Associate III
June 17, 2014
Posted on June 18, 2014 at 01:10

Thanks so much for your code. I finally tried it, but how come I get data jumping from 7000-51000. Is this normal?

Also, how did you know to write 0x20C7, then 0xAB00?

From datasheet below I don't see anything like it.

http://www.st.com/web/en/resource/technical/document/datasheet/CD00135460.pdf