Skip to main content
Senior III
June 21, 2017
Question

STM32F401VE and boot mode

  • June 21, 2017
  • 4 replies
  • 1216 views
Posted on June 21, 2017 at 15:04

Hi,

I've purchased the STEVAL-3DP001V1 board from ST, which is powered by a STM32F401VE. There is a jumper called boot which is wired as follow:

0690X00000607KwQAI.png

So the pin BOOT0 is normally held high when the jumper is not fitted. BOOT1 is PB2 which is tied to ground.

0690X00000607L1QAI.png

According to the F401 user manual, the uC will boot from system memory when the jumper is not fitted, and from main flash memory when fitted.

My question is: what happens once the uC has boot in system memory ? Will it stay there forever, waiting for stimuli on any of the enabled communication peripherals ?

#steval-3dp001v1 #boot #stm32f401
This topic has been closed for replies.

4 replies

shorai
Associate III
February 13, 2019

Hi Kraal

I know this is an old post

Any joy with getting this board working?

I can connect and navigate through wifi, but none of the buttons work.

I put in an SD card per the specs

I also tried connecting using the st-link vcomm port and get what look like baud rate errors.

The software does not load, per the instruction, int STSW / AC6 - the directories are all over the place as is the case with any eclipse based tools

Grrrrrrr

any help appreciated

thanks in advance

Chris

KraalAuthor
Senior III
February 13, 2019

Hi Chris,

I did not work much on it. I am using TrueStudio 9 and since I take this project as a learning exercise, I must say that for the moment not much is being done.

Although, like you, I don't like when the source code is spread in different directoriews when not necessary, I am writing my own C code to suit my liking.

I have initialized all the I/Os, the 2 USARTs (one for the ST-Link VCOM at 230400 bps and the other for the WiFi module at 115200 bps). I also set the communication with the motor drivers and currently can read back their status.

I did not tried the original Marlin firmware with motors connected so I can't tell if the buttons were active or not, but I had the impression that there was no communication between the wifi and the F401 (again, not verified).

Sorry that I can't help you much with that. My goal is to make a hot wire foam cutter from scratch, so it takes me time to make any progress...

shorai
Associate III
February 13, 2019

Hi Kraal,

Thanks for the quick answer, I really appreciate it.

Just knowing that someone else is having the SAME problem is an advantage.

The next problem I face is that ither SW4ST (AC6) nor True Studio seem to work with the files on the GIT.

I have had endless problems in the past with anything Eclipse based as the directories do not come across correctly and you end up with both missing includes as well as virtual file link problems (file does not exist) .

I'm going to bring the source into a more standard makefile structure, or create my own TrueStudio project and copy the files I need into it and see where that gets me.

I might also look for the eclipse XML files and edit those as the eclipse editor seems a little broken in that regard

I'll keep you posted

Chris

KraalAuthor
Senior III
February 14, 2019

Thanks, I'll follow your progress. In the meantime I asked about the wifi module and how to modify the web server. It may be useful for you,you can check it there https://community.st.com/s/question/0D50X00009vLs22SAC/customizing-web-pages-on-the-spwf01sa

Again I did not have the time to actually test it...

Best regards

Kraal