Associate III
September 14, 2016
Question
HAL_TIM_Base_Start_DMA - STM32CubeMX
- September 14, 2016
- 4 replies
- 2903 views
Posted on September 14, 2016 at 12:27
I've try to use HAL_TIM_Base_Start_DMA with TIM6.
To configure the system I'm using STM32CubeMX. We I start the project I can't receive any interrupt...HELP.In Attachment the ioc file.My change after code generation:In red tim.c file modify:#include ''tim.h''#include ''dma.h''/* USER CODE BEGIN 0 */uint32_t aCCValue_Buffer[3] = {10000, 1000, 100};
/* USER CODE END 0 */... /* Peripheral interrupt init */ HAL_NVIC_SetPriority(TIM6_IRQn, 0, 0); HAL_NVIC_EnableIRQ(TIM6_IRQn); /* USER CODE BEGIN TIM6_MspInit 1 */HAL_TIM_Base_Start_DMA(tim_baseHandle, aCCValue_Buffer, 3);
/* USER CODE END TIM6_MspInit 1 */..../* USER CODE BEGIN 1 */void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim) {
HAL_GPIO_TogglePin(LD2_GPIO_Port, LD2_Pin);}/* USER CODE END 1 */