Question
STM32F215 SWD connexion impossible
Posted on November 11, 2014 at 14:32
Hi all,
Our new board arrived yesterday but I can't even connect via SWD. Could you please help us to find the problem ?BOOT0 = pull down via external 10K resistorBOOT1 = direct connexion to GNDSWD are well routed, but I can't see any level on the SWD pins : 0V on every pin.When the ST-Link v2 is acting on JTRST : no response from MCU.The same problem is encountered on 2 different boards.We tried with NRST pin floating, or with NRST in direct connection to VDD : same behaviour...What do you think about please ?[EDIT] = no response too by USART1 bootloader...