Skip to main content
hisham23
Associate III
November 5, 2012
Solved

Stm32f105 don't enter dfu mode

  • November 5, 2012
  • 2 replies
  • 1211 views
Posted on November 05, 2012 at 11:29

Hello,

I designed a board which contains stm32f105 microcontroller, and i want to use DFU as bootloader in order to download my program to the micro controller through usb port.

I put BOOT0 =1, and BOOT1=0

PA10=PD6=PB5=0

then i powered the circuit and connected it to usb port of my pc which runs windows xp.

But the pc didn't recognise a new device.

These are the processor data:

STM32F105

VCT6        Z

990TD   93

MYS 99 045

First question: Why the pc didn't recognize a new device?

Second question: the date code is 045 what year does this mean?

Regards,

Hisham
    This topic has been closed for replies.
    Best answer by hisham23
    Posted on November 07, 2012 at 11:22

    Hello,

    Finally the problem is solved.

    I connected pin 1 of the usb (power =5v) from computer directly to USB_VBUS pin PA9 in stm32f105 instead of connecting it through 20kOhm resistor and it works!

    2 replies

    hisham23
    hisham23AuthorBest answer
    Associate III
    November 7, 2012
    Posted on November 07, 2012 at 11:22

    Hello,

    Finally the problem is solved.

    I connected pin 1 of the usb (power =5v) from computer directly to USB_VBUS pin PA9 in stm32f105 instead of connecting it through 20kOhm resistor and it works!
    Visitor II
    November 8, 2024

    I have the stm32f107 that has troubled me for the past few days. This resolved my issue.  Thanks from the future