Skip to main content
eyals111
Associate II
February 4, 2014
Solved

difference ReadBinary() to ExtendedReadBinary()

  • February 4, 2014
  • 1 reply
  • 743 views
Posted on February 04, 2014 at 16:21

hi ,

What is the main difference between   ReadBinary()  to ExtendedReadBinary()  ?

for what i understand is that ExtendedReadBinary() ignore Message length  (but still reside in the Memory address).

is this the only difference ?

#m24sr #extendedreadbinary
This topic has been closed for replies.
Best answer by Anais GALLIGANI
Posted on February 07, 2014 at 18:01

Hi ,

ReadBinary command only allows to read the NDEF message of the file (limit is given in NDEF message length = 2 first bytes of the file).  But this lets unused memory area at the end of the NDEF file.

To be able to read beyond NDEF message, M24SRxx-Y products offer a proprietary command: ExtendedReadBinary command.

This command can read the bytes beyond NDEF message, until the end of the file.

I hope this is clear,

Best regards,

Have a nice day,

ST NFC/RFID Dynamic tag support

hi ,

What is the main difference between   ReadBinary()  to ExtendedReadBinary()  ?

for what i understand is that ExtendedReadBinary() ignore Message length  (but still reside in the Memory address).

is this the only difference ?

1 reply

Anais GALLIGANI
Anais GALLIGANIBest answer
Visitor II
February 7, 2014
Posted on February 07, 2014 at 18:01

Hi ,

ReadBinary command only allows to read the NDEF message of the file (limit is given in NDEF message length = 2 first bytes of the file).  But this lets unused memory area at the end of the NDEF file.

To be able to read beyond NDEF message, M24SRxx-Y products offer a proprietary command: ExtendedReadBinary command.

This command can read the bytes beyond NDEF message, until the end of the file.

I hope this is clear,

Best regards,

Have a nice day,

ST NFC/RFID Dynamic tag support

hi ,

What is the main difference between   ReadBinary()  to ExtendedReadBinary()  ?

for what i understand is that ExtendedReadBinary() ignore Message length  (but still reside in the Memory address).

is this the only difference ?