Associate II
July 9, 2012
Question
spi interrupt problem for lsm330dl
- July 9, 2012
- 9 replies
- 2573 views
Posted on July 09, 2012 at 12:33
i try to use the spi interrupt , but the whole program just hanged at case 101 which is in the void GYRO_Task(void), it shows me ''+++''. anything wrong?
here is some part of my code. #ifdef GYRO_SPI_USE_INTERRUPT NVIC_InitStructure.NVIC_IRQChannel = SPI2_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); #endifvoid GYRO_Trigger_Read(uint16_t HalfWord, unsigned char *rxdataptr)
{ HalfWord = HalfWord << 8; HalfWord |= 0x8000;GYRO_TxData = HalfWord;
GYRO_RxDataPtr = rxdataptr;#ifdef GYRO_SPI_USE_INTERRUPT
SPI_I2S_ITConfig(GYRO_SPI, SPI_I2S_IT_TXE, ENABLE); SPI_I2S_ITConfig(GYRO_SPI, SPI_I2S_IT_RXNE, ENABLE); #endifGYRO_CS_LOW();
}void GYRO_Interrupt_SetRxData(unsigned char tempchar)
{ *GYRO_RxDataPtr = tempchar; GYRO_Operation_State = 0; }char GYRO_Interrupt_GetTxData(void)
{ return GYRO_TxData; }