Skip to main content
timon1994
Associate II
June 26, 2012
Question

Controller resets when enabling interrupt

  • June 26, 2012
  • 2 replies
  • 686 views
Posted on June 26, 2012 at 12:33

controller resets when I enable timer interrupt with the period about half second.

watchdog is ok.

timer config:

TIM_TimeBaseInitTypeDef  TIM_TimeBaseStructure;

RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM6, ENABLE);

TIM_TimeBaseStructInit(&TIM_TimeBaseStructure);

TIM_TimeBaseStructure.TIM_Period = 10000;

TIM_TimeBaseStructure.TIM_Prescaler = 16800-1;

TIM_TimeBaseInit(TIM6, &TIM_TimeBaseStructure);

TIM_ITConfig(TIM6, TIM_IT_Update, ENABLE);

TIM_Cmd(TIM6, ENABLE);

enabling interrupt:

NVIC_EnableIRQ(TIM6_DAC_IRQn);

also I've tried to enable interrupt this way:

NVIC_InitTypeDef NVIC_InitStructure;

NVIC_InitStructure.NVIC_IRQChannel = TIM6_DAC_IRQn;

NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0;

NVIC_InitStructure.NVIC_IRQChannelSubPriority = 1;

NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;

NVIC_Init(&NVIC_InitStructure);

interrupt handler:

void TIM6_DAC_IRQnHandler() {

   if (TIM_GetITStatus(TIM6, TIM_IT_Update) != RESET) {

      TIM_ClearITPendingBit(TIM6, TIM_IT_Update);

      IWDG_ReloadCounter();

   }

}

what can I do?

thanks in advance.
    This topic has been closed for replies.

    2 replies

    frankmeyer9
    Associate III
    June 26, 2012
    Posted on June 26, 2012 at 14:41

    what can I do?

     

    Attach a debugger, and see what actually happens.

    Read out the RCC_CSR register, it should tell you what did reset the uC, if at all.

    Tesla DeLorean
    Guru
    June 26, 2012
    Posted on June 26, 2012 at 15:02

    The interrupt handlers must match the names specified in the vector table so instead of

    void TIM6_DAC_IRQnHandler() {

    ...

    use

    void TIM6_DAC_IRQHandler() {

    ...

    Confirm you are using the correct startup_stm32f1xx_xx_xx.s file for your specific part.
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..