Skip to main content
tarzan2
Associate III
July 4, 2014
Question

LSM303D temperature format

  • July 4, 2014
  • 2 replies
  • 642 views
Posted on July 04, 2014 at 15:19

Hello,

I got good results reading accelerometer data but the temperature register is about 36 (decimal), the datasheet mentions 8LSB/°C, 36/8 = 4.5°C, this is quite cold ;)

Room temp is 24°C, the other sensors located near the LSM are indicating 28°C.

What is the good conversion factor?
This topic has been closed for replies.

2 replies

jamesjames9
Visitor II
July 14, 2016
Posted on July 14, 2016 at 03:09

Hi,

I see there has been no replies to your post for the past 2 years.

Check out this disappointing answer by Miroslav from ST:

/71915817

ST Employee
August 12, 2016
Posted on August 12, 2016 at 09:27

Unfortunately

 the temperature sensor can be used only to measure temperature variations. It isn't suitable to return absolute temperatures measures. The value represents difference respect to a reference not specified value.

Best regards

Miroslav