stm32L476 buggy package
Dear all,
During a porting of an RTOS on a Discovery 476 board I discovered a serious problem with the stm32l476xx.h file provided by ST. All the elements of timers structure are defined as a 32-bits. So, after having spent a couple of hours in debugging my porting I discovered that some elements HAVE to be accessed in a
16-bits
and not in a32-bits
. In particular, the SR register accessed in 32-bits crashe my system with an 'Hard Fault Exception'. In the documentation the SR register is described to be 16-bits. So, I modified the original structure of the package and now everything work as expected. Here is my modification.The original package (that crash the interruption acknowledge)
typedef struct {
...
volatile
uint32_t
SR;...
} TIM_TypeDef;
The modified package (that works)
typedef struct {
...
volatile
uint16_t
SR;volatile
uint16_t
RESERVED0;...
} TIM_TypeDef;
I pointed different peripheral structures and I discovered that potentially I can have the same problem (of course, this depends on how the silicon supports the 32-bit accesses for 16-bit wide registers).
Now I have serious doubts regarding the quality of the packages provided by ST!
Regards
Edo