Skip to main content
angel2
Explorer
August 1, 2012
Question

USB3340 from SMSC allways working in FS usin a STM32F407

  • August 1, 2012
  • 2 replies
  • 773 views
Posted on August 01, 2012 at 18:11

Hi All,

I have developed a PCB that contains an USB3340 and a STM32F407, using the: STM32_USB-Host-Device_Lib_V2.1.0. But is allways working as a FS device instead of a HS one. I have tried the same code in the STM3240 eval board, and works really fine.

Can someone help me?? Have someone find (and solved) the same problem??

I will really appreciate some answer, because a don't know what more to do...

Thanks in advance!!
    This topic has been closed for replies.

    2 replies

    Tesla DeLorean
    Guru
    August 1, 2012
    Posted on August 01, 2012 at 20:18

    I have developed a PCB that contains an USB3340 and a STM32F407, using the: STM32_USB-Host-Device_Lib_V2.1.0. But is allways working as a FS device instead of a HS one. I have tried the same code in the STM3240 eval board, and works really fine.

    So not a software issue then, how about on a reference design using the SMSC part?

    Providing a snap shot of your schematic might provide for more informed discussion.
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    ian2399
    Associate
    August 9, 2012
    Posted on August 09, 2012 at 14:12

    You're not the only one. See thread 'STM32F2/F4 problams with various ULPI USB PHYs'

    You can find it by seaching forums for ChirpK.

    Regards

    Ian