Question
Displaying icon on TFT ?
Posted on April 14, 2014 at 10:18
Guys,
Does anyone of you know on how to display array of bitmap to TFT LCD ? I tried :
void LCD_DrawBMPFromFile()
{
char temp_buffer[100],line[512];
int count,bmpData,bmpAddr;
const int icon[220] =
{
0x42,0x4D,0xC6,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x76,0x00,0x00,0x00,0x28,0x00,0x00,0x00,0x0A,
0x00,0x00,0x00,0x0A,0x00,0x00,0x00,0x01,0x00,0x04,0x00,0x00,0x00,0x00,0x00,0x50,0x00,0x00,0x00,
0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,
0x00,0x00,0x00,0x80,0x00,0x00,0x80,0x00,0x00,0x00,0x80,0x80,0x00,0x80,0x00,0x00,0x00,0x80,0x00,
0x80,0x00,0x80,0x80,0x00,0x00,0x80,0x80,0x80,0x00,0xC0,0xC0,0xC0,0x00,0x00,0x00,0xFF,0x00,0x00,
0xFF,0x00,0x00,0x00,0xFF,0xFF,0x00,0xFF,0x00,0x00,0x00,0xFF,0x00,0xFF,0x00,0xFF,0xFF,0x00,0x00,
0xFF,0xFF,0xFF,0x00,0xFF,0xFF,0xFF,0xFF,0xFF,0x00,0x00,0x00,0xFF,0xFF,0xFF,0xFF,0xFF,0x00,0x00,
0x00,0xFF,0xFF,0xFF,0xFF,0xFF,0x00,0x00,0x00,0x99,0x99,0x99,0x9F,0xFF,0x00,0x00,0x00,0x99,0x99,
0x99,0x9F,0xFF,0x00,0x00,0x00,0x99,0x99,0x99,0x9F,0xFF,0x00,0x00,0x00,0x99,0x99,0x99,0x9F,0xFF,
0x00,0x00,0x00,0x99,0x99,0x99,0x9F,0xFF,0x00,0x00,0x00,0x99,0x99,0x99,0x9F,0xFF,0x00,0x00,0x00,
0x99,0x99,0x99,0x9F,0xFF,0x00,0x00,0x00};
//write LCD RAM here
LCD_WriteRAM_Prepare(); /* Prepare to write GRAM */
LCD_Clear(Yellow);
for (bmpAddr; bmpAddr < 100; bmpAddr += 2)
{
bmpData = (uint16_t)(*(icon + bmpAddr)) + (uint16_t)((*(icon + bmpAddr + 1)) << 8);
LCD_WriteRAM( bmpData );
}
__inline void LCD_WriteRAM(uint16_t RGB_Code)
{
/* Write 16-bit GRAM Reg */
LCD_RAM = RGB_Code;
}
but got no response, any clues ? thanks