Associate III
April 19, 2017
Question
STM32F429 USB and FMC interoperability problem
- April 19, 2017
- 1 reply
- 774 views
Posted on April 19, 2017 at 15:45
I am trying to use SDRAM (42S16400J) and NOR flash (M29W256GL) with STM32F429. With the code I generated with STM32CubeMX, Flash and SDRAM are working without problems. When I add USB-FS-OTG (device) to the project, the processor is blocked. The code is running when I turn off flash and SDRAM initialize operations. But with the first FMC operation I made while adding USB OTG to the project, the processor is blocked. I would like you to share if there is any reasoning about this problem.
Thank you