Skip to main content
kinovicf
Associate II
February 8, 2013
Question

Unique 96bit ID meaning and its shortening

  • February 8, 2013
  • 11 replies
  • 5869 views
Posted on February 08, 2013 at 08:06

Hello.

I have a question concerning processor 96bit UID. I understand that this number is ST unique number and I would like to use it as a board identification in production. But the number is farly long for expressing in text form. So I would like to short it to be unique relative for certain chip.

I see that DFU boatloader uses a shorter serial number similar to UID and it differs among similar chips. Would anybody know the number meaning  or a mask reducing the number to demanded purpose?

Thank you.

#id-unique-meaning-shortening
    This topic has been closed for replies.

    11 replies

    kinovicf
    kinovicfAuthor
    Associate II
    February 20, 2013
    Posted on February 20, 2013 at 09:13

    Hello.

    Thanks for the link. The 96bit UID looks to be combination of lot number, waf number and X,Y position on it. I found out how DFU serial number is probably created (tested on some chips F2 and F4).

    Here is example for F4 (UID expressed hexadecimally in MSb (bits 95-0)) :

    UID: | 31 34 35 33 | 31 31 47 0B | 00 23 00 38 |

    and

    DFU s/n: ''3157356B3131'',

    where:

    ''31'' = 0x31 (bits 95-88)

    ''57'' = 0x34 (bits 87-80) + 0x23 (bits 23-16)

    ''35'' = 0x35 (bits 79-72)

    ''6B'' = 0x33 (bits 71-64) + 0x38 (bits 7-0)

    ''31'' = 0x31 (bits 63-56)

    ''31'' = 0x31 (bits 55-48)

    It is a question if the same serial number could be created from different lot number and X, Y position.

    Tesla DeLorean
    Guru
    February 20, 2013
    Posted on February 20, 2013 at 19:06

    It is a question if the same serial number could be created from different lot number and X, Y position.

     

    Always hard to represent a 96-bit value using 24/48-bits. I don't think anyone here has enough data to provide a through solution. I wouldn't rely on a truncated value being unique. Output the number in base64 or something, surely 16 characters can't be too much to handle on the test/pc side.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    emalund
    Associate III
    February 20, 2013
    Posted on February 20, 2013 at 20:21

    I do not know about this chip, but previously - with another chip - asking ''your'' question, the reply was ''we can in no way guarantee anything re using a shortened number''.

    I would be VERY weary of using a partial number.

    anyhow, if this might be a solution Mzxim has a <$0.50 ''unique serial number'' chip (If I recall DS1452) that only uses 48 bits

    Erik

    kinovicf
    kinovicfAuthor
    Associate II
    March 25, 2013
    Posted on March 25, 2013 at 11:25

    Thanks for the posts. I have already decided not to ignore any data of 96-bit number.

    Andrew Neil
    Super User
    March 25, 2013
    Posted on March 25, 2013 at 15:31

    ''I would be VERY weary of using a partial number''

    You should be very wary of using a partial number - otherwise you are likely to become very weary of the consequences...!

    ;)

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
    denis
    Associate III
    September 24, 2013
    Posted on September 24, 2013 at 16:16

    Just to make sure: ST provided libs do not define some magic macro / function for this uid (or address of)  (and flash size ..), without me coding in the number from the manual?

    (just in case there is a macro/func I can't find, i've searched UID on all their support lib for f10xxx ..  but other family also prob have uid? f2xxx ? )

    Tesla DeLorean
    Guru
    September 24, 2013
    Posted on September 24, 2013 at 17:19

    Just to make sure: ST provided libs do not define some magic macro / function for this uid (or address of)  (and flash size ..), without me coding in the number from the manual?

     

     

    (just in case there is a macro/func I can't find, i've searched UID on all their support lib for f10xxx ..  but other family also prob have uid? f2xxx ? )

    I'm not aware of a macro, the addresses are different across each series, and sometimes within (L1). The different parts also have different ROM(OTP) locations. Read the documentation carefully, observe the non-linear addressing.

    I would certainly try to sanity check the FLASH size value before accepting the UID, and have the code warn on the part, as well as any test fixturing app if it saw any anomalies or duplicated UID.

    The UID is not acceptable as a MAC address, but could be used in encryption related to key or salting applications. Storing your own GUID and/or MAC in OTP is probably another way to go.

    I think the key take away is to OWN and VALIDATE your solution, and not abdicate that to any ST library function.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    denis
    Associate III
    September 25, 2013
    Posted on September 25, 2013 at 12:17

    >I'm not aware of a macro, the addresses are different across each series,  ...different ROM locations.....

    Precisely : I thought such macro/func of theirs should do, have right address depending on my device (depending on my project macro i guess...).

    I find lots of, imho 'useless' little funcs in that ST lib, like a function to read CCR1 register for example.

    >and sometimes within (L1)

    What is L1 ? Low power mode family?

    denis
    Associate III
    September 25, 2013
    Posted on September 25, 2013 at 12:25

    > duplicated UID.

    Well that id is good for shyte..    Is this something known to happen?

    At least from the STM32F1 manual, there is very strong emphasis on uniqueness.

    ''The 96-bit unique device identifier provides a reference number which is unique for any

     

    device and in any context. These bits can never be altered by the user.

    The 96-bit unique device identifier can also be read in single bytes/half-words/words in

     

    different ways and then be concatenated using a custom algorithm.''