Skip to main content
usafape
Associate II
Sep 12, 2012 6:10 AM UTC
Question

RAM access by address

Posted on September 12, 2012 at 08:10

Hi,

I want to have the ability to read/write to a specific address in RAM. How could I do that in C.

Any suggestions?

#really-bad-idea
    This topic has been closed for replies.

    10 replies

    frankmeyer9
    Associate III
    Sep 12, 2012 6:58 AM UTC
    Posted on September 12, 2012 at 08:58

    I suggest the stm32fxxx.h files as an example, like stm32f10x.h for the F1 family.

    This file(s) are found in the standard peripheral libs for the specific part, and declare all fixed peripheral addresses/registers by laying C struct over them.

    It is your turn, however, to make sure that you do not interfere with the compiler/linker.

    konoppo
    Associate II
    Sep 12, 2012 7:15 AM UTC
    Posted on September 12, 2012 at 09:15

    Are you sure you can't do it in other way? Writing to a fixed address is often not good idea. The best way to do it is modification of the linker script. You have to:

    - reduce the .bss section to make some RAM free

    - make a new section in this place starting from YOUR_ADDRESS, call it for example .reserved-ram

    Now you can simply read or write to/from the address which is in range of your section and you don't need to worry if there are any variables inside:

    ((uint8_t *) *(YOUR_ADDRESS + 0x01)) = i;

    You can also declare the variable like that:

    uint8_t ReservedRam[256] __attribute__((section(''.reserved-ram'')));

    and this

    i = ReservedRam[3];

    reads the byte from YOUR_ADDRESS + 0x03. 

    Best regards

    Konoppo

    usafape
    usafapeAuthor
    Associate II
    Sep 12, 2012 8:01 AM UTC
    Posted on September 12, 2012 at 10:01

    Looks like I found the solution:

    uint32_t *pointer;
    uint32_t pi,pii;
    //SAVING DATA
    pi = 0x20000000;//RECEIVE ADDRESS AND SAVE IT INTO A INTEGER
    pointer = (uint32_t*)pi; //CONVERT IT INTO POINTER
    *pointer = 100; //SAVE 100 INTO POINTER (0X20000000)
    //RETRIEVING DATA
    pi = 0x20000000;//RECEIVE ADDRESS AND SAVE IT INTO A INTEGER
    pointer = (uint32_t*)pi; //CONVERT IT INTO POINTER
    pii = *pointer;//READING ADDRESS THRU THE POINTER

    My linker file will have allocated region for this so the compiler won't mess around (hopefully).
    frankmeyer9
    Associate III
    Sep 12, 2012 11:50 AM UTC
    Posted on September 12, 2012 at 13:50

    Something I don't understand: what is your point in knowing the address ?

    A variable, and it's name, are an abstraction explicitely provided for this issue. You refer to to a memory location by the name of the variable. You neither need to know, nor to care at which address it is actually located. That task  is left to the compiler and the linker.

    usafape
    usafapeAuthor
    Associate II
    Sep 13, 2012 2:37 PM UTC
    Posted on September 13, 2012 at 16:37

    It has to do with giving flexibility to the system design. If I have access to an specific address, then I only have one command from an external domain to read/write to that address.

    Also, I can use the same command to control other configuration registers and so on.

    I basically have control over the processor's brain in real time ;)

    David Littell
    Senior II
    Sep 13, 2012 5:43 PM UTC
    Posted on September 13, 2012 at 19:43

    Are you thinking of something like the old BASIC PEEK and POKE commands?

    Andrew Neil
    Super User
    Sep 13, 2012 6:32 PM UTC
    Posted on September 13, 2012 at 20:32

    ''I basically have control over the processor's brain in real time''

     

    More to the point, there is a veryhigh risk that you will totally derange the processor by messing with its brain carelessly and/or inappropriately!!

    Sure, it can be done - but that does not mean that it should be done!
    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
    emalund
    Associate III
    Sep 13, 2012 6:42 PM UTC
    Posted on September 13, 2012 at 20:42

    It has to do with giving flexibility to the system design

     

     

    WRONG

    It has to do with inflexibility to the system design.

    you will have to dig out your hex calxulator every darn time you add a variable

    Erik
    Tesla DeLorean
    Guru
    Sep 13, 2012 11:07 PM UTC
    Posted on September 14, 2012 at 01:07

    //SAVING DATA

        *((uint32_t *)0x20000000) = 100;

    //RETRIEVING DATA

        pii = *((uint32_t *)0x20000000);

    If fixed/known addresses are required, perhaps it would be better to use definition files, or linker scripts

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    frankmeyer9
    Associate III
    Sep 14, 2012 6:50 AM UTC
    Posted on September 14, 2012 at 08:50

    I basically have control over the processor's brain in real time ;)

     

    I think you don't actually want this..

    But you can implement a virtual machine. That let's you control all 'fixed' addresses in the memory space of the virtualized processor, while leaving actual physical addresses to the compiler and linker.