Skip to main content
juergen239955_stm1
Associate II
August 31, 2012
Question

ST application note AN3116: referenced examples cannot be found

  • August 31, 2012
  • 4 replies
  • 1398 views
Posted on August 31, 2012 at 02:57

After reviewing the (very informative) application note on ''STM32's ADC modes

and their applications'', which is located at the site below, I was curious where I can find the numerous examples which are referenced in the note, and which allegedly are attached to it. Examples are:

- Dual_FastInterleaved, page 10

- Dual_AlternateTrigger, page 13

- Dual_Combined_Reg_Inj_Sumultaneous, page 14,  ... etc.

Thanks for your help,

JJ

http://www.st.com/internet/com/TECHNICAL_RESOURCES/TECHNICAL_LITERATURE/APPLICATION_NOTE/CD00258017.pdf

    This topic has been closed for replies.

    4 replies

    Tesla DeLorean
    Guru
    August 31, 2012
    Posted on August 31, 2012 at 03:23

    A lot of the examples have percolated into the standard peripheral library example files.

    Are you looking for the STM32F1xx parts or the more recent F2 or F4?

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Tesla DeLorean
    Guru
    August 31, 2012
    Posted on August 31, 2012 at 05:24

    After a bit of Googling I have this

    http://www.st.com/internet/com/SOFTWARE_RESOURCES/SW_COMPONENT/FIRMWARE/an3116.zip

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    juergen239955_stm1
    Associate II
    September 6, 2012
    Posted on September 06, 2012 at 23:22

    Muchos gracias! Exactly what I was looking for (exact version not so important, I just wanted to see the implementation as guidance).

    Thanks again.

    nanayakkaraan
    Associate III
    August 14, 2013
    Posted on August 14, 2013 at 13:41

    Hello,

    At the moment I could not find sample Firmware in the given location, instead I came across those in the following location.

    http://www.st.com/web/catalog/tools/FM147/CL1794/SC961/SS1743/PF257864

    May be ST have shifted the location.

    Anyway thought it would be helpful to share this location, for the sake of someone else searching for the samples.

    :)

    Thanks.

    -Anuradha.