Question
Bit set/reset timing
Posted on May 18, 2014 at 09:52
I am doing some work which requires precise timing and I think the STM8S can do what I need. In order to prove this I setup a simple program which toggles PD0 in a while loop.
I am using the IAR compiler and it compiles the following:
PD_ODR = 0;
PD_ODR = 1;to:
clr PD_ODR
mov PD_ODR, ♯?b1The clear instruction operates in 1 clock cycle but the mov takes 2 cycles. I decided to try the inline assembler and changed the C statement to:
asm(''bres PD_ODR, &sharp0'');
asm(''bset PD_ODR, &sharp0'');PM0044 states that these instructions should take 1 cycle each but they both appear to take 2 cycles.
Has anyone seen this? I'm wondering if PM0044 is correct.Regards,Mark #timing-stm8s-instruction