Skip to main content
thln47
Associate III
Dec 8, 2015 9:20 AM UTC
Question

bug on STM32_USB_Device_Library

Posted on December 08, 2015 at 10:20

Hi,

I found another bug on USB library for the STM32F3XX (STM32_USB_Device_Library in STM32Cube_FW_F3_V1.3.0).

STM32Cube_FW_F3_V1.3.0\Middlewares\ST\STM32_USB_Device_Library\Core\Src\usbd_core.c

In the usbd_core.c file, the function �USBD_LL_SetupStage� should check the bits [D6:D5] of bmResquest to identify the type request. The function doesn�t work for non standard request type. See USB2.0 specification chapter 9.3 table 9.2.

So when I send to the device request with bmResquest =0xA2 (Dir=In, Type=Class, Recipient=Endpoint) used in USBTMC stack (USBTMC_InitiateAbortBulkOut), this request is badly parsed!

Here is the right code for this function:

/**

* @brief  USBD_SetupStage

*         Handle the setup stage

* @param  pdev: device instance

* @retval status

*/

USBD_StatusTypeDef USBD_LL_SetupStage(USBD_HandleTypeDef *pdev, uint8_t *psetup) {

    USBD_ParseSetupRequest(&pdev->request, psetup);

    pdev->ep0_state = USBD_EP0_SETUP;

    pdev->ep0_data_len = pdev->request.wLength;

    /* bug should check if bmRequest is standard request type ! */

    /* @see table 9.2 chap 9 of USB Spec ! */

    uint8_t type = pdev->request.bmRequest & USB_REQ_TYPE_MASK;

    switch (type) {

    case USB_REQ_TYPE_STANDARD:

        switch (pdev->request.bmRequest & 0x1F)

        {

        case USB_REQ_RECIPIENT_DEVICE:

            USBD_StdDevReq(pdev, &pdev->request);

            break;

        case USB_REQ_RECIPIENT_INTERFACE:

            USBD_StdItfReq(pdev, &pdev->request);

            break;

        case USB_REQ_RECIPIENT_ENDPOINT:

            USBD_StdEPReq(pdev, &pdev->request);

            break;

        default:

            USBD_LL_StallEP(pdev, pdev->request.bmRequest & 0x80);

            break;

        }

        break;

    case USB_REQ_TYPE_CLASS:

    case USB_REQ_TYPE_VENDOR:

        /* added missing callback ! */

        if (pdev->dev_state == USBD_STATE_CONFIGURED) {

            if (pdev->pClass->Setup != NULL)

                pdev->pClass->Setup(pdev, &pdev->request);

        } else {

            USBD_CtlError(pdev, &pdev->request);

        }

        break;

    }

    return USBD_OK;

}

This bug is also on all firmware.

#setupstage #bug #usb #stm32cube
This topic has been closed for replies.

1 reply

Nickname5522_O
Visitor II
Dec 10, 2015 2:39 PM UTC
Posted on December 10, 2015 at 15:39

Hi ln.thierry,

It is right that the check of bmResquest's bits is missing, but it should be done in ''USBD_StdDevReq'', ''USBD_StdItfReq'' and ''USBD_StdEPReq'' functions.

The issue is reported to development team.

Thank you for all your feedback and contribution :-).

-Shahrzad-