Question
STM32 USART3
Posted on August 02, 2013 at 06:30
Hello All,
I am using USART3 in Half duplex mode for 1 wire protocol. The reset pulse of the one wire protocol has to be sent at 9600 and data exchnage at 115200. The problem I am facing here is BRR register doesnt get updated with baud rates. HSE_VALUE is 8Mhz SYSCLK(Hz) |64000000 APB1 prescalar is 16 I am not getting the proper baud rate and hence i get just 0 from 1 wire slave. Could anyone pls help in resolving this issue . Thanks #usart-rcc #stm32