Question
STM32F4 External 3.6V power
Posted on June 11, 2012 at 09:32
Hi,
I was wondering if I can power the Discovery board via the VDD pins on the headers? I want to use 3.6V rather than the 3V used so I can get a larger more accurate ADC reading (0-3V6 rather than 0-3V). How would this work if I want to program using USB while 3.6V is active? Also, I need the PC to be isolated from the board during debug/programming (ADC will be referenced to 3-phase GND). I was thinking of making an isolated USB cable (as in the following link), will this work? http://www.analog.com/static/imported-files/newsletters/digital_isolation/USB_cable_Nappnote_Rev_d.pdf Thanks for your help in advance.