Associate
July 1, 2012
Question
Real-time command execution STM32F407
- July 1, 2012
- 5 replies
- 1797 views
Posted on July 01, 2012 at 13:57
Hi, everyone.
Testing STM32F407. Runs it at 168 MHz (5.92 ns cycle), FLASH-> ACR = FLASH_ACR_DCEN | FLASH_ACR_ICEN | FLASH_ACR_PRFTEN | FLASH_ACR_LATENCY_5WS. Outstanding at the PA1 a simple square wave:PM_(RCC->AHB1ENR, RCC_AHB1ENR_GPIOAEN) = 1; // GPIOA clock enabled
PM_(GPIOA->MODER, GPIO_MODER_MODER1_0) = 1; // PA1 - General purpose output mode GPIOA->OSPEEDR |= GPIO_OSPEEDER_OSPEEDR1; // PA1 - 100 MHz High speed while (1) { GPIOA-> BSRR = GPIO_BSRR_BS_1; GPIOA-> BSRR = GPIO_BSRR_BR_1; GPIOA-> BSRR = GPIO_BSRR_BS_1; GPIOA-> BSRR = GPIO_BSRR_BR_1; GPIOA-> BSRR = GPIO_BSRR_BS_1; GPIOA-> BSRR = GPIO_BSRR_BR_1; GPIOA-> BSRR = GPIO_BSRR_BS_1; GPIOA-> BSRR = GPIO_BSRR_BR_1; GPIOA-> BSRR = GPIO_BSRR_BS_1; GPIOA-> BSRR = GPIO_BSRR_BR_1; } Compiled as follows:STR r1, [r0, ♯ 0x18]
STR r2, [r0, ♯ 0x18] STR r1, [r0, ♯ 0x18] STR r2, [r0, ♯ 0x18] STR r1, [r0, ♯ 0x18] STR r2, [r0, ♯ 0x18] STR r1, [r0, ♯ 0x18] STR r2, [r0, ♯ 0x18] STR r1, [r0, ♯ 0x18] STR r2, [r0, ♯ 0x18] B | L1.6 | On the oscilloscope can see this signal (Attachments img) https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Attachments/23318/01.png This means that the Branch instruction is actually executed in 3 cycles? I have to debug in Keil stm32f4discovery. At the Branch instruction cycle counter in the Keil (States) increased by 1. In addition, using SysTick and DWT-> CYCCNT, they are also incremented by 1 for instructions Branch. Why is it so? #art-gpio-ahb