Skip to main content
thommagn
Associate II
June 18, 2012
Question

Writing to flash problem

  • June 18, 2012
  • 1 reply
  • 615 views
Posted on June 18, 2012 at 18:45

Hi,

I tried one of the flash examples for the STM32f4 Discovery. First i tried to read from adress 0x80E0000, then i tried to write to that same adress. After this, when I try to debug, i got the error ''No source available for ''0xfffffffe'' ''.

So I tried strapping 3V3 to boot0 and reseting it. When I try to debug now, I get stuck at:

  b  LoopCopyDataInit

and I am unable to start the debug (Stuck at this position and unable to pause debugger). At this point I tried to do a full chip erase, which lead me back to the 0xfffffffe error as mentioned above. I've tried to debug different projects that I know is working but with the same results.

Do anyone have ideas of what i might have done to my discovery?

Thanks
    This topic has been closed for replies.

    1 reply

    Tesla DeLorean
    Guru
    June 18, 2012
    Posted on June 18, 2012 at 20:24

    The error means you are trying to step into code for which the debugger has no source to display. ie you've put code on it jumping to some odd location, or is just buggy.

    Make sure BOOT0 is not high. Use the ST-Link utilities, and erase the device.

    Try downloading an eval of Keil or IAR, and try those.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..