Skip to main content
johnsotack9
Associate III
February 12, 2013
Question

Constant Data at Fixed Flash Address.

  • February 12, 2013
  • 3 replies
  • 885 views
Posted on February 12, 2013 at 22:33

I have a boot loader that resides in the first flash block of an STM32F4 family processor which is 16K begining at 0x08000000.  I would like the last four byte of the sector at 0x08003ffc to contain constant data representing a version number.

Any suggestions?  I am using Atollic tools which are GCC based.  I would prefer a C/C++ solution but could use assembler if necessary.  My current knowlege of ARM assembly is fairly limited.

John
    This topic has been closed for replies.

    3 replies

    Tesla DeLorean
    Guru
    February 12, 2013
    Posted on February 12, 2013 at 22:52

    Any suggestions?

    Specify an address, or memory/section in the linker script, and define the ''attributes'' of the variable to direct it's placement.

    Google some documentation and examples for GNU linker scripts.
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    johnsotack9
    Associate III
    February 13, 2013
    Posted on February 13, 2013 at 16:40

    Thanks.  If I make one section just for the version, that should work.

    John

    johnsotack9
    Associate III
    February 13, 2013
    Posted on February 13, 2013 at 22:29

    I used the interupt vectors as an example for the linker file (to define a section similar to

    .isr_vector

    ) and the startup.s file (to defined data within the section as is done with the vector table).  The defined values showed up in the s-record at the expected address.

    John