Question
Wakeup from SPI question
Posted on June 29, 2014 at 17:28
I would like to wake up from SPI communication (using the NSS pin).
I have the NSS line connected to both PA0 and the SPI(3) NSS pin. I would like to wake up from either stop mode or stanby mode (preferably standby mode) while not loosing the data sent to me. is that possible? if so, how? I'm running STM32F405, at 84MHz. I know it is possible in other M4 core processor but couldn't figure out how to do it in this one. Thank you #wakeup #stop #spi #standby