Associate III
July 18, 2015
Question
can over run
- July 18, 2015
- 7 replies
- 2160 views
Posted on July 18, 2015 at 19:02
i using stm23f429 as can controller for servo drive
but some time i have over run problem. i check the signals by oscope and understood that , some time fifo of canbx dose not being empty even a can massage transmit correctly and respond is recieved please see attached pic d1-> can_rx d0->can_tx 1->canh 2->canl for example in the pic i need send just one massage to node id 0x620 but i send three massage as the same correctly