Question
STM32F4 /F7 USB HS PHY max speed
Posted on February 10, 2016 at 11:29
Hi,
at the moment im using a STM32F3 as custom FS HID device to send 1000 64byte packets each second (64kb/s) to host pc. i would like to increase the speed so im wondering which speed i can get with the external ulpi HS PHY on F4 and F7 eval boards with hid and perhaps cdc? is it possible to get the maximum of three 1024 byte packets in each 125ms microframe? thanks!