Skip to main content
stenasc
Associate III
April 18, 2017
Question

Hard Fault When I enable the USART3_8_IRQn interrupt.

  • April 18, 2017
  • 5 replies
  • 1117 views
Posted on April 18, 2017 at 23:07

Hi Forum,

I'm using the stm32f091, but when I enable the USART3 interrupt, the system hard faults. I already use USARTS1 and 2 without any problem. Not sure what else is required, so I'd be grateful for some assistance. One thing I;d like to know is  how do you distinguish between interrupts from USARTS3 up to USART8.

Kind Regards

Bob

  USART_InitTypeDef USART_InitStructure;

  GPIO_InitTypeDef GPIO_InitStructure;

  NVIC_InitTypeDef NVIC_InitStructure;

  // Enable GPIOC clock

  RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOC, ENABLE);

 

  // Enable USART3 APB clock

  RCC_APB1PeriphClockCmd(RCC_APB1Periph_USART3, ENABLE);

    

 

  // Connect pin to Periph

  GPIO_PinAFConfig(GPIOC, GPIO_PinSource10, GPIO_AF_1);   //  USART3 TX

  GPIO_PinAFConfig(GPIOC, GPIO_PinSource11, GPIO_AF_1);   //  USART3 RX

 

  // Configure pins as AF pushpull

  GPIO_InitStructure.GPIO_Pin = GPIO_Pin_10 | GPIO_Pin_11;

  GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;

  GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;

  GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;

  GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_DOWN;

  GPIO_Init(GPIOC, &GPIO_InitStructure);

      

  USART_InitStructure.USART_BaudRate = 9600;

  USART_InitStructure.USART_WordLength = USART_WordLength_8b;

  USART_InitStructure.USART_StopBits = USART_StopBits_1;

  USART_InitStructure.USART_Parity = USART_Parity_No;

  USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;

  USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;

  USART_Init(USART3, &USART_InitStructure);

    

  USART_Cmd(USART3, ENABLE);

      

//  Enable the COM3 Receive interrupt: this interrupt is generated when the

//  COM3 receive data register is not empty

  USART_ITConfig(USART3, USART_IT_RXNE, ENABLE);

  // USART3 IRQ Channel configuration

  NVIC_InitStructure.NVIC_IRQChannel = USART3_8_IRQn;   

  NVIC_InitStructure.NVIC_IRQChannelPriority = 1;

  NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;

  NVIC_Init(&NVIC_InitStructure);
    This topic has been closed for replies.

    5 replies

    Tesla DeLorean
    Guru
    April 18, 2017
    Posted on April 19, 2017 at 00:23

    You check the status registers of the USART you plan to service. 

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    stenasc
    stenascAuthor
    Associate III
    April 18, 2017
    Posted on April 19, 2017 at 01:17

    Fair enough regarding the usart article status register but any idea why the hard fault occurs.

    Bob

    waclawek.jan
    Super User
    April 19, 2017
    Posted on April 19, 2017 at 01:25

    Make sure the ISR's name matches that in the vector table, typically located with startup code.

    JW

    stenasc
    stenascAuthor
    Associate III
    April 19, 2017
    Posted on April 19, 2017 at 14:38

    Thanks very much. The interrupt was missing from the vector table. Adding it fixed the issue. Once again many thanks to the forum.

    Kind Regards

    Bob