Skip to main content
berge472
Associate
May 16, 2013
Question

Flashing form windows command line

  • May 16, 2013
  • 1 reply
  • 2066 views
Posted on May 16, 2013 at 18:53

I have a project where I will need to flash a few hundred chips that are already on boards. I have set up a chain programmer which is controlled by an MCU. basically it is just a chain of sockets for the boards that all get connected to an st-link v2, and it sequentially powers up the boards and runs a bat file to flash them. But I cant seem to find any information on using the st-link utility in windows command line. I use it linux, but this project will be used by our assembly department and they all run windows 7.

Does anyone have any information on using the st-flash in command line on windows?
    This topic has been closed for replies.

    1 reply

    Amel NASRI
    ST Technical Moderator
    June 5, 2013
    Posted on June 05, 2013 at 11:41

    Hello,

    You can use the ST-LINK Utility command line interface (CLI).

    See

    http://www.st.com/st-web-ui/static/active/en/resource/technical/document/user_manual/CD00262073.pdf

     for more details on how to do it.

    Regards,

    ST.MCU

    To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.