Skip to main content
stenasc
Associate III
December 12, 2012
Question

spi eeprom reading problem

  • December 12, 2012
  • 6 replies
  • 1624 views
Posted on December 13, 2012 at 00:57

Hi,

I am writing data into an ST 95M02SPI eeprom memory, from a STM32F051 micro but I am unable to read it back. On the scope I can see the proper data on MISO (just an incrementing count). SCK looks to be fine, (stops after LSB on MISO) and CS goes high just after that. However, I just can't read the returned value into the main app. All I read is 00h

It looks as if MISO data is not being shifted in the shift register or RXFIFO just contains all zeros.Using the SPI_Config function below was the only way I could get the SPI signals to show anything.  If anyone could help, I'd greatly appreciate it. I'm using the SPI2 port on the microcontroller.

void SPI_Config(void)

{

  SPI_InitTypeDef SPI_InitStructure;

  GPIO_InitTypeDef GPIO_InitStructure;

    /* Enable SPI clock, SPI2 */

  RCC_APB1PeriphClockCmd(RCC_APB1Periph_SPI2, ENABLE);    

        

  /* SPI pin mappings */

  GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;

  GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;

  GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_DOWN;

  GPIO_InitStructure.GPIO_Speed = GPIO_Speed_Level_1;

  /* SPI SCK pin configuration */

  GPIO_InitStructure.GPIO_Pin = GPIO_Pin_13;

  GPIO_Init(GPIOB, &GPIO_InitStructure);

  /* SPI MOSI pin configuration */

  GPIO_InitStructure.GPIO_Pin = GPIO_Pin_15;    

  GPIO_Init(GPIOB, &GPIO_InitStructure);

    

  /* SPI MISO pin configuration */    

  GPIO_InitStructure.GPIO_Pin = GPIO_Pin_14;

  GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN;

  GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP;    // This needs to have a PULL-UP

  GPIO_Init(GPIOB, &GPIO_InitStructure);

 

  // Configure CS pin as output floating

  GPIO_InitStructure.GPIO_Pin = GPIO_Pin_12;

  GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT;

  GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP;

  GPIO_Init(GPIOB, &GPIO_InitStructure);    

        

 

  /* SPI configuration -------------------------------------------------------*/

  SPI_I2S_DeInit(SPIx);

  SPI_InitStructure.SPI_Direction = SPI_Direction_2Lines_FullDuplex;

  SPI_InitStructure.SPI_Mode = SPI_Mode_Master;

  SPI_InitStructure.SPI_DataSize = SPI_DataSize_8b;

  SPI_InitStructure.SPI_CPOL = SPI_CPOL_Low;

  SPI_InitStructure.SPI_CPHA = SPI_CPHA_1Edge;

  SPI_InitStructure.SPI_NSS = SPI_NSS_Soft;

  SPI_InitStructure.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_4;

  SPI_InitStructure.SPI_FirstBit = SPI_FirstBit_MSB;

 

  SPI_Init(SPIx, &SPI_InitStructure);

  SPI_SSOutputCmd(SPIx, ENABLE);

  SPI_Cmd(SPIx, ENABLE);    

    

}

uint8_t SPI_Flash_Read(uint8_t ins, uint8_t address)

{

uint8_t spi_rd_data_local;

  

      EEPROM_CS_LOW;

    // Send SPI instruction         

    SPI_SendData8(SPIx, ins);    

      while (SPI_I2S_GetFlagStatus(SPIx, SPI_I2S_FLAG_TXE) != SET);

    // Send SPI address H

    SPI_SendData8(SPIx, 0x00);

    while (SPI_I2S_GetFlagStatus(SPIx, SPI_I2S_FLAG_TXE) != SET);    

    // Send SPI address M

    SPI_SendData8(SPIx, 0x00);

    while (SPI_I2S_GetFlagStatus(SPIx, SPI_I2S_FLAG_TXE) != SET);    

    // Send SPI address

    SPI_SendData8(SPIx, address);

    while (SPI_I2S_GetFlagStatus(SPIx, SPI_I2S_FLAG_TXE) != SET);    

      // Send Dummy Byte for Clocks

    SPI_SendData8(SPIx, 0xFF);

      // Now sit back and wait for the data

    while (SPI_I2S_GetFlagStatus(SPIx, SPI_I2S_FLAG_RXNE) == RESET);

        

    spi_rd_data_local = SPI_ReceiveData8(SPIx);                

    while (SPI_I2S_GetFlagStatus(SPIx, SPI_I2S_FLAG_BSY) == SET);

    EEPROM_CS_HIGH;

        printf(''\n\r Local Read Data Received = %.2X'', spi_rd_data_local);

        

    return (spi_rd_data_local);

}
    This topic has been closed for replies.

    6 replies

    Tesla DeLorean
    Guru
    December 13, 2012
    Posted on December 13, 2012 at 02:20

    As a blind build I might offer this, I think you need to watch RXNE as it only gets cleared if you actually read the data register, so in your case you get some prior data.

    Your BUSY was waiting on SPI1?

    /* Enable SPI clock, SPI2 */
    RCC_APB1PeriphClockCmd(RCC_APB1Periph_SPI2, ENABLE); 
    /* SPI SCK, MOSI, MISO pin configuration */
    GPIO_InitStructure.GPIO_Pin = GPIO_Pin_13 | GPIO_Pin_15 | GPIO_Pin_14;
    GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
    GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
    GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_DOWN;
    GPIO_InitStructure.GPIO_Speed = GPIO_Speed_Level_1; // 10 MHz
    GPIO_Init(GPIOB, &GPIO_InitStructure);
    // Configure CS pin as output floating
    GPIO_InitStructure.GPIO_Pin = GPIO_Pin_12;
    GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT;
    GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP;
    GPIO_Init(GPIOB, &GPIO_InitStructure); 
    GPIO_PinAFConfig(GPIOB, GPIO_PinSource13, GPIO_AF_0); // SPI2 SCK
    GPIO_PinAFConfig(GPIOB, GPIO_PinSource15, GPIO_AF_0); // SPI2 MOSI
    GPIO_PinAFConfig(GPIOB, GPIO_PinSource14, GPIO_AF_0); // SPI2 MISO
    /* SPI configuration -------------------------------------------------------*/
    SPI_I2S_DeInit(SPIx);
    SPI_InitStructure.SPI_Direction = SPI_Direction_2Lines_FullDuplex;
    SPI_InitStructure.SPI_Mode = SPI_Mode_Master;
    SPI_InitStructure.SPI_DataSize = SPI_DataSize_8b;
    SPI_InitStructure.SPI_CPOL = SPI_CPOL_Low;
    SPI_InitStructure.SPI_CPHA = SPI_CPHA_1Edge;
    SPI_InitStructure.SPI_NSS = SPI_NSS_Soft;
    SPI_InitStructure.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_4;
    SPI_InitStructure.SPI_FirstBit = SPI_FirstBit_MSB;
    SPI_Init(SPIx, &SPI_InitStructure);
    SPI_SSOutputCmd(SPIx, ENABLE);
    SPI_Cmd(SPIx, ENABLE); 
    }
    uint8_t SPI_SendByte(uint x)
    {
    while(SPI_I2S_GetFlagStatus(SPIx, SPI_I2S_FLAG_TXE) == RESET); // TX Empty (Front Test)
    SPI_SendData8(SPIx, x); 
    while(SPI_I2S_GetFlagStatus(SPIx, SPI_I2S_FLAG_RXNE) == RESET); // Wait for data to shift out
    return(SPI_ReceiveData8(SPIx)); // Read to clear RXNE
    }
    uint8_t SPI_Flash_Read(uint8_t ins, uint8_t address)
    {
    uint8_t spi_rd_data_local;
    EEPROM_CS_LOW;
    // Send SPI instruction 
    SPI_SendByte(ins); 
    // Send SPI address H
    SPI_SendByte(0x00);
    // Send SPI address M
    SPI_SendByte(0x00);
    // Send SPI address
    SPI_SendByte(address);
    // Send Dummy Byte for Clocks
    spi_rd_data_local = SPI_SendByte(0xFF);
    while (SPI_I2S_GetFlagStatus(SPIx, SPI_I2S_FLAG_BSY) == SET);
    EEPROM_CS_HIGH;
    printf(''
    
     Local Read Data Received = %.2X'', spi_rd_data_local);
    return (spi_rd_data_local);
    }

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    jpeacock2399
    Associate III
    December 13, 2012
    Posted on December 13, 2012 at 15:57

    /** 
    * @brief Shift data in/out 
    * @param Iob pointer to I/O control block 
    * @param pData data to shift out 
    * @retval data read by shift out 
    * 
    * This routine shifts out one byte and returns the data shifted in. 
    */ 
    static unsigned char SpiDev_Shift(SpiDev_IOB *Iob, unsigned char pData) 
    { 
    unsigned char i; 
    // make sure shift register empty 
    while(SPI_I2S_GetFlagStatus(Iob->Info.SPIx, SPI_I2S_FLAG_TXE) == RESET) 
    { // clear any pending shift out/in 
    while(SPI_I2S_GetFlagStatus(Iob->Info.SPIx, SPI_I2S_FLAG_RXNE) == SET) 
    { // empty rx buffer 
    i = SPI_I2S_ReceiveData(Iob->Info.SPIx); // clear SPI buffer 
    if( SPI_I2S_GetFlagStatus(Iob->Info.SPIx, SPI_I2S_FLAG_OVR) == SET) 
    spiOvers[Iob->Info.SpiPort]++; // count overruns, reset 
    } 
    } // shift register cleared 
    // shift out one byte, shift in one byte 
    SPI_I2S_SendData(Iob->Info.SPIx, pData); // Send byte to the SPI peripheral 
    while(SPI_I2S_GetFlagStatus(Iob->Info.SPIx, SPI_I2S_FLAG_RXNE) == RESET) ; // wait for data shifted in 
    i = SPI_I2S_ReceiveData(Iob->Info.SPIx); // empty SPI buffer 
    if( SPI_I2S_GetFlagStatus(Iob->Info.SPIx, SPI_I2S_FLAG_OVR) == SET) 
    spiOvers[Iob->Info.SpiPort]++; // count overruns, reset 
    return i; 
    } 

    There are two issues you need to check. The first is making sure the RXNE stays clear so you don't have a RX overrun. This is the routine I use to send and receive on SPI. The second issue has to do with your EEPROM. You need to check the SPI timing for the clock edge when data is clocked in and out of the part. A problem with the ST SPI hardware is that it only handles one clock edge (CPOL setting) for read and write, so parts that require different clock edges for read (typically falling edge)and write (typically rising edge)are somewhat complicated to use with the STM If this is the case you need to change CPOL clock polarity between read and write. Jack Peacock
    stenasc
    stenascAuthor
    Associate III
    December 13, 2012
    Posted on December 13, 2012 at 20:12

    Hi Clive

    Thanks for that. It tidied it up but  I still read 00h. Again I still see the correct data from the EEprom. It seems to me that a lot of zero bytes have been clocked into the RX buffer and I'm reading these, but I'm not sure. So, I'm using Clive's read function and my SPI Write functions looks like. All help is appreciated.

    uint8_t SPI_Flash_Write(uint8_t ins, uint8_t address, uint8_t data)

    {

      

        EEPROM_CS_LOW;    

        SPI_SendByte(ins);    

        SPI_SendByte(0x00);

        SPI_SendByte(0x00);

        SPI_SendByte(address);

        SPI_SendByte(data);

            while (SPI_I2S_GetFlagStatus(SPIx, SPI_I2S_FLAG_BSY) == SET);

        EEPROM_CS_HIGH;        

            

         return (1);

    }

    void WriteEnable(void)

    {

        EEPROM_CS_LOW;

        SPI_SendData8(SPIx, 0x06);    

        // Wait for SPI Tx buffer empty

        while (SPI_I2S_GetFlagStatus(SPIx, SPI_I2S_FLAG_TXE) != SET);

            // Clear receive buffer

        Clr_Rcv_Buf();    

        EEPROM_CS_HIGH;              

    }

    void Clr_Rcv_Buf(void)

    {

    uint8_t spi_rd_data;    

         // Clears the receive buffer

        if (SPI_I2S_GetFlagStatus(SPIx,SPI_I2S_FLAG_RXNE) == SET)

           spi_rd_data = SPI_ReceiveData8(SPIx);    

    }

    My main calling routine is

    for (ee_add = 0; ee_add<128; ee_add++)

      {

      WriteEnable();        

      spi_wr_flag = SPI_Flash_Write(0x02, ee_add, ee_add);

      Delay(100);        

      }

        printf(''\n\r Flash Write Complete'');

        

       

    for (ee_add = 0; ee_add<128; ee_add++)

      {        

      spi_rd_data = SPI_Flash_Read(0x03, ee_add);

        Delay(100);              

      }    

    stenasc
    stenascAuthor
    Associate III
    December 13, 2012
    Posted on December 13, 2012 at 20:15

    Hi Jack,

    I'll check out the polarity issue on the datasheet. This may be indeed valid, but I would expect to see at least something returned, not all zeros.

    stenasc
    stenascAuthor
    Associate III
    December 14, 2012
    Posted on December 14, 2012 at 13:39

    Hi Lads,

    Thanks for the help. Working perfectly now. It was the receive flag that was causing the bother.

    fang
    Visitor II
    March 21, 2014
    Posted on March 21, 2014 at 09:28

    Hi, clive! I have the same problem, I got always 0 for the variable status. When I made the main.c file, there was a warning ''variable status was set but never used'' which calls my attention. But I always cant find the problem, here is my code, could you help?

    static __IO uint32_t TimingDelay; void spiInit(void); uint8_t Send( uint8_t data); void spiInit() { GPIO_InitTypeDef GPIO_InitStruct; SPI_InitTypeDef SPI_InitStruct; /*Enable peripheral clock for SPI1*/ RCC_APB2PeriphClockCmd(RCC_APB2Periph_SPI1, ENABLE); /* Enable SCK, MOSI and MISO GPIO clocks */ RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE); /* define a variable of type GPIO_InitTypeDef* */ GPIO_InitStruct.GPIO_Pin = GPIO_Pin_5 | GPIO_Pin_7 | GPIO_Pin_6; GPIO_InitStruct.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStruct.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStruct.GPIO_OType = GPIO_OType_PP; // this sets the pin type to push / pull (as opposed to open drain) GPIO_InitStruct.GPIO_PuPd = GPIO_PuPd_DOWN; // this sets the pullup / pulldown resistors to be active GPIO_Init(GPIOA, &GPIO_InitStruct); /* Configure GPIO PIN for Lis Chip select */ //on fait deux fois GPIO_Init() ? Pin NSS est bien Slave Select, il faut utiliser!http://en.wikipedia.org/wiki/Serial_Peripheral_Interface_Bus// GPIO_InitStruct.GPIO_Pin = GPIO_Pin_10; GPIO_InitStruct.GPIO_Mode = GPIO_Mode_OUT; GPIO_InitStruct.GPIO_PuPd = GPIO_PuPd_UP ; GPIO_Init(GPIOA,&GPIO_InitStruct); /* choose alternate function 0 for certain pins */ GPIO_PinAFConfig(GPIOA, GPIO_PinSource5, GPIO_AF_0); GPIO_PinAFConfig(GPIOA, GPIO_PinSource6, GPIO_AF_0); GPIO_PinAFConfig(GPIOA, GPIO_PinSource7, GPIO_AF_0); /* using the SPI_Init() function to do the initialization */ //Program the Polarity, Phase, First Data, Baud Rate Prescaler, Slave // Management, Peripheral Mode and CRC Polynomial values //SPI_I2S_DeInit(SPI1); SPI_InitStruct.SPI_Mode = SPI_Mode_Master; SPI_InitStruct.SPI_Direction = SPI_Direction_2Lines_FullDuplex; SPI_InitStruct.SPI_DataSize = SPI_DataSize_8b; SPI_InitStruct.SPI_CPOL = SPI_CPOL_Low; SPI_InitStruct.SPI_CPHA = SPI_CPHA_1Edge; SPI_InitStruct.SPI_NSS = SPI_NSS_Soft; SPI_InitStruct.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_8; SPI_InitStruct.SPI_FirstBit = SPI_FirstBit_MSB; SPI_Init(SPI1,&SPI_InitStruct); SPI_SSOutputCmd(SPI1, ENABLE); /* Enable the SPI */ SPI_Cmd(SPI1, ENABLE); /* Configure the FIFO threshold to select at which threshold the RXNE event is generated */ SPI_RxFIFOThresholdConfig(SPI1, SPI_RxFIFOThreshold_QF); //XNE event is generated if the FIFO level is greater or equal to 1/4// /* send data */ GPIO_SetBits(GPIOA,GPIO_Pin_10); //test if the flag related set?// } uint8_t Send( uint8_t data) { SPI_SendData8(SPI1, data); while( SPI1->SR & SPI_I2S_FLAG_BSY ); // wait until SPI is not busy anymore //Delay(1); return SPI_ReceiveData8(SPI1); } /** * @brief Inserts a delay time. * @param nTime: specifies the delay time length, in 1 ms. * @retval None */ void Delay(__IO uint32_t nTime) { TimingDelay = nTime; while(TimingDelay != 0); } /** * @brief Decrements the TimingDelay variable. * @param None * @retval None */ void TimingDelay_Decrement(void) { if (TimingDelay != 0x00) { TimingDelay--; } } /** * @brief Decrements the TimingDelay variable. * @param None * @retval None */ int main(void) { /*!< At this stage the microcontroller clock setting is already configured, this is done through SystemInit() function which is called from startup file (startup_stm32f0xx.s) before to branch to application main. To reconfigure the default setting of SystemInit() function, refer to system_stm32f0xx.c file */ /* Add your application code here */ RCC_ClocksTypeDef RCC_Clocks; /* SysTick end of count event each 1ms */ RCC_GetClocksFreq(&RCC_Clocks); SysTick_Config(RCC_Clocks.HCLK_Frequency / 1000); spiInit(); /* Infinite loop */ while (1) { uint8_t status = 0; GPIO_WriteBit(GPIOA, GPIO_Pin_10, Bit_RESET); Send(0x05); status = Send(0xFF); GPIO_WriteBit(GPIOA, GPIO_Pin_10, Bit_SET); } }