Associate III
September 26, 2017
Question
Timer output don't stop
- September 26, 2017
- 0 replies
- 601 views
Posted on September 26, 2017 at 12:09
I am doing a program where I have a 50Hz square signal and a PWM to generate a sinusoidal with 90 points. Each time
the signal edge of 50Hz is raised or lowered, the timer must be reset and start a new modulation. However, the first two values do not match the programmed width.

The modulation starts correctly on the third pulse, and when there is this displacement the modulation does not end correctly. This is the code: This is the external interrupt, for sync my 50Hz signal.
void EXTI15_10_IRQHandler(void)
{
//PB10 50H+input float int
//PB11 50H-input float int
if(EXTI_GetITStatus(EXTI_Line10) != RESET)
{
if(MAR==1){
//port_set(PORT_B, 15, 1); //MAR ON
port_set(PORT_A, 4, 1); //ON 50Hz
//TIM2->CCR1=0;
portsONtimer();
}
EXTI_ClearITPendingBit(EXTI_Line10);
}
if(EXTI_GetITStatus(EXTI_Line11) != RESET)
{
if(MAR==1){
port_set(PORT_A, 4, 0); //OFF 50Hz
portsONtimer();
}
//port_set(PORT_A, 4, 0); //OFF 50Hz
EXTI_ClearITPendingBit(EXTI_Line11);
}
}�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
This is the timer controlling the PWM:
void TIM2_IRQHandler(void)
{
//static int indice = 0;
TIM2->SR &= ~(1<<0); // clear UIF flag- bit0
switch(dir){
case 0:
if(indice==89){ //change direction of the table
dir= 1;
}
TIM2->CCR1=frec50[indice]; //Increasing table, 1/4 sine
break;
case 1:
if(indice==89){ //change direction of the table
dir= 0;
stop_timer();
}
TIM2->CCR1=frec50[PWM_ELEMENTS - indice - 1];//Decreasing table, 2/4 sine
break;
}
indice = (indice + 1) % PWM_ELEMENTS;
}�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
And this is the function that starts timer:
void portsONtimer(void){
//GPIOA->CRL = (GPIOA->CRL & 0xFFFFFFF0 | 0x00000003); //PA0.1
//port_set(PORT_A, 0, 0); //S
dir= 0;
indice=0;
TIM_Cmd(TIM2, ENABLE);
//TIM2->CCR1=0;
TIM2->CNT = 0;
GPIOA->CRL = (GPIOA->CRL & 0xFFFFFFF0 | 0x0000000B); //PA0
} �?�?�?�?�?�?�?�?�?�?�?
And the stoptimer:
void stop_timer(void){
TIM2->CCR1=0; //negat
//TIM1->CCR2=0;
TIM_Cmd(TIM2, DISABLE);
port_set(PORT_A, 0, 0); //S
GPIOA->CRL = (GPIOA->CRL & 0xFFFFFFF0 | 0x00000003); //PA0.1
TIM2->CNT = 0;
indice=0;
dir= 0;
TIM2->CCR1=0;
}
�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
Any idea? Thank you very much. Daniel Prieto