Skip to main content
John Craven
Senior
April 3, 2018
Question

Intermittently switching a PWM/ONESHOT timer output to high impedance

  • April 3, 2018
  • 6 replies
  • 1476 views
Posted on April 03, 2018 at 16:05

I have read a few short posts around this forum, that suggest disabling a timer in PWM/OC mode, will change the output pins to high impedance.

As background, I am trying to interface with a device that requires a PWM control pulse 500-2500us width as an input signal at 50-100Hz, The device replies with telemetry, on the same line, by creating a brief 1us wide pulse on the same line. The timing between the end of the control input pulse and the brief telem pulse determines the telem value (0.5ms equals zero and 5.5ms is fullscale). There is a cycle of 11 telem values. The cycle start is marked, by the device not sending a telem pulse, followed by 11 replies. 

Device interface spec, includes that i must yield the line (high impedance) after generating the control pulse and use a 2k pullup on my end for my 3.3V logic.

I would like to send the control input pulse using a ONESHOT mode timer that is triggered based on another timer that is not relevant to this discussion.

If i disable the ONESHOT timer at the end of its pulse (end of pulse callback), will its output go high impedance? I have a scheme, based on another input capture timer to measure the telem value timing and on its input capture callback, can i simply re-enable the ONESHOT timer and have it ready for the next trigger event?

I am looking for confirmation from somebody who has done something similar or can confirm that temporarily disabling a timer changes it output to high impedance and simple re enable will reverse that and timer will function on next event.

If disabling the timer, does not set out to High impedance, i am open to suggestions. Obviously, i can add external components, tristate buffer/driver, but i am looking for soft solution before adding hardware.

    This topic has been closed for replies.

    6 replies

    waclawek.jan
    Super User
    April 3, 2018
    Posted on April 03, 2018 at 16:21

    It's not the *timer* you are going to enable/disable, but the *channel*, using its respective TIMx_CCER.CCyE bit. The timer itself remains to run and react etc., so when reenabling you may perhaps want to reset TIMx_CR1.CEN and TIMx_CNT too.

    There are other ways to skin the cat, of course, e.g. changing AF to Input in GPIO, or changing timer mode from output compare to input capture in TIMx_CCMR. More options are available in the Advanced Timers (TIM1, TIM8), see TIMx_BDTR and TIMx_CR2; but you probably don't want to go that far.

    JW

    John Craven
    Senior
    April 3, 2018
    Posted on April 03, 2018 at 16:43

    Thank you Jan.

    I can try disabling the channel instead.

    I was going to use a retriggerable one pulse mode mode timer for the outgoing control pulse.

    The channel won't get disabled until the pulse finish callback.

    Correct me if i am wrong, but i think the timer CNT is reverent until the next trigger.

    The CNT stops at ARR when the pulse completes and stays there until the next trigger. I have solid control of the upstream trigger.

    The channel should be re-enabled long before the  next trigger occurs.

    If i was using PWM, then i agree, i probably would have to massage other things like the CNT.

    waclawek.jan
    Super User
    April 3, 2018
    Posted on April 03, 2018 at 16:47

    The channel should be re-enabled long before the  next trigger occurs.

    Then it's just the simple matter of TIMx_CCER.CCyE.

    JW