Skip to main content
paker earth
Associate II
March 20, 2017
Question

Could mcp3208 chip connect to stm32 pins directly?

  • March 20, 2017
  • 1 reply
  • 667 views
Posted on March 20, 2017 at 15:48

Hi all

This's datasheet for reference.

http://ww1.microchip.com/downloads/en/DeviceDoc/21298c.pdf

 

Could I use it directly without any level shifter for 3v3v to 5v?

Can someone kindly tell me where to lookup the information?

Is the Digital IO part or not? I can't understand the description clearly.

Thank you all in advance. 

0690X00000606T9QAI.png
    This topic has been closed for replies.

    1 reply

    waclawek.jan
    Super User
    March 22, 2017
    Posted on March 22, 2017 at 10:18

    According to that datasheet, MCP320x could be operated at the same supply voltage as STM32, say 3.3V, with reduced sampling rate, then you don't need level shifts.

    If you'd insist on using 5V supply for the MCP320x, I'd recommend to use level shifts, even if it might work marginally without them.

    JW