Associate
January 8, 2017
Question
X-NUCLEO-CCA02M1 Expansion sample program problem
- January 8, 2017
- 2 replies
- 1545 views
Posted on January 08, 2017 at 07:42
I have got a strange problem with X-NUCLEO-CCA02M1 expansion board interfacing with NUCLEO-L476RG. I have followed
quick start guide to test the functionality of MEMS mic through the audacity(v2.1.2) software as mentioned in doc. I have loaded the test binaries to the X-NUCLEO-L476RG and I am able to get the device recognized as �STM32 AUDIO Streaming in FS Mode� both in my device manager and Audacity software�s microphone list. Now when I start recording in Audacity I get random signals not even close to a normal sound waveform. I have also attached the screenshot of what I am getting along with waveforms of sound I recorded with my internal mic array. I have very little knowledge of internal programming of the test application but consulting Getting started guide section 3.4.2.2 I can confirm the jumper connections on board are exactly same as mentioned in this section. I have checked on two windows based machines one is running windows 10 64-bit and other windows 7 64-bit but results are same. I am looking forward for your guidelines to debug the issue. I am sure there is nothing wrong in compiled binaries as I am getting Audio device recognized, I suspect this could be a hardware issue.#cca02m1-memsmic1 #steval-boards-for-mems-mics