Skip to main content
frankyang9
Associate
Jul 21, 2016 5:45 AM UTC
Question

Help: About operating temperature of STM32F302VDH6/STM32F302VDT6/STM32F302VDT6TR

Posted on July 21, 2016 at 07:45

Dear Sirs,

On the web page http://www.st.com/content/st_com/en/products/microcontrollers/stm32-32-bit-arm-cortex-mcus/stm32f3-series/stm32f302/stm32f302vd.html

Says the  operating temperature of STM32F302VDH6/STM32F302VDT6/STM32F302VDT6TR is from -40 ~105 degree, but from the datasheet of these P/N, it's -40~85 degree, which is true?

Thanks a lot,

Best Regards

Frank 

#temperature
    This topic has been closed for replies.

    2 replies

    Nesrine M_O
    Associate
    Jul 21, 2016 9:02 AM UTC
    Posted on July 21, 2016 at 11:02

    Hi Frank, 

    Welcome to STM32 community!

    On the web page, it says that the STM32F302xD/E family operates in the -40 to +85°C and -40 to +105°C temperature ranges from a 2.0 to 3.6 V power supply.

    On the STM32F302xD STM32F302xE datasheet rev3 says the same message on the Description paragraph and on the General operating conditions table.

    As it is described in the General operating conditions table we can reach 105°C for 6 suffix version in Low power dissipation state, please refer to your datasheet for more details. 

    -Syrine-

    frankyang9
    Associate
    Jul 21, 2016 11:42 AM UTC
    Posted on July 21, 2016 at 13:42

    Hi Syrine,

    Thanks for the information. In the v3.0 datasheet, for example, if the package is LQFP100, we should calculate the PDmax of MCU, and following the figure 69 to find out the Ta, correct? So as U say, it's possible that Ta of the suffix 6 can be larger than 85 degree when MCU runs in low power mode.

    But the figure 69 says the max Ta of suffix 6 is 105 degree when Pdmax = 0mW, I think it's meaningless in actual product design. 

    Is my understanding correct?

    Best Regards

    Frank